Part Number: TPS63020
Hi,
I am troubled that the phase margin of TPS63020 can only be about 30 deg.
Please tell me how to improve the phase margin. Also, please tell me how much phase margin is required.
Best Regards,
Hasegawa
Hello Users,
TI Resource Explorer upgraded to version 4.0 recently and some of the links referencing Resource Explorer Projects and Labs are no longer working. This is currently a known issue and TI is working to address this.
In the meantime, one…
FAQ: Logic and Voltage Translation > Input Parameters >> Current FAQ
The most common example of this question comes from the fact that Standard Logic devices are specified at 1.65V, 3V, and 4.5V, however most engineers use our devices at 1.8V, 3.3V…
Part Number: AWR1642 Other Parts Discussed in Thread: IWR1642 , AWR1843 , , IWR1443 , AWR1443 This thread applies to AWR1443, AWR1642, AWR1843 and to the industrial variants IWR1443, IWR1642.
The following file has been updated to check the Temperature…
FAQ: Logic and Voltage Translation > Quality and Manufacturing >> Current FAQ
TI's General Quality Guideline (page 7) describes our official policy on obsoleting a device. This policy is summarized below.
TI's Product withdrawal/discontinuance process…
Part Number: BQ24610 Other Parts Discussed in Thread: BQ24650 , BQ24617
What are some key considerations when designing a schematic using BQ24610 or BQ24650, and what can I do if I want to simplify external component count by disabling some features…
Part Number: ISO224 Other Parts Discussed in Thread: , TLV6001 , OPA277
This might be a silly question, but is there any problem that might arise when tying the negative output of ISO224 to the low-side ground, GND2? My original plan was to do this…
Part Number: TPS63001 Other Parts Discussed in Thread: TPS63802 , TPS63000
Hi all,
Currently we are using TPS63001 fixed 3.3V output DC-DC Converter. As per the TPS63001 DC-DC converter datasheet, module taking Quiescent current (Iq) is less than…