Part Number: AM2612
Hi experts, I see that the AM26x devices support Inter-Processor Communication between multiple R5F cores and include a mechanism to maintain shared memory across cores. What is recommended for my multi-core applications? When do…
Part Number: MSPM33C321A
Per ARM architecture, VTOR must be aligned to:
Alignment = Power of 2 ≥ (Number of vectors × 4)
For MSPM33C321A:
- ICTR register = 1 → Hardware supports 53 external IRQs (IRQ0- 52 )
- Total vectors = 16 (system exceptions…
Part Number: INA236 Other Parts Discussed in Thread: INA3221 , INA209 , , INA228 , INA237
I want to use the ALERT pin of a digital power monitor, what should I pay attention to?
Part Number: AM2434
While the existing OSPI driver implements XIP mode functionality, the default Flash parts (S28HS512T and S25HL512T) available on AM24x, AM64x, AM62x, and AM275x boards, do not support Read-While-Write (RWW) operations or multi-bank…
Part Number: TPS3842
I need to monitor and sequence 3 power supply rails. The main bus voltage in my design is 12V, followed by LDOs for 5V, 3.3V, and 1.8V. Can please provide the simplest solution? Also board size is very limited so I need smallest…
Part Number: MSPM0-SDK
This thread is used to update the software or hardware update for application note of Low cost AC motor control solution based on MSPM0 and Triac.
5466.Resource_HW&FW.zip
Part Number: CC2674P10 Other Parts Discussed in Thread: CC2674R10 , CC1314R10 , CC1354P10 , CC1354R10 , CC2755R10 , CC2755P10
Q1: What security features are available on CC2674 and CC13x4 devices?
A: The CC2674 and CC13x4 (CC2674R10, CC2674P10, CC1314R10…
Part Number: TDA4VL-Q1
What is the effort required by the system integrator to enable and test ECC on the different IPs on the SoC using ECC aggregators?
Part Number: INA228 Other Parts Discussed in Thread: SYSCONFIG
I’m reading the current register value, but the result is wrong. Why am I not reading the value that I expect to be reading?
Part Number: BQ25785EVM Other Parts Discussed in Thread: BQ25785 , BQSTUDIO
Please see attached for the BQ25785 BQZ file to be used with BQSTUDIO software.
To use the GUI you will need to download Battery management studio software from TI.com, then…