Part Number: TDA4VM Tool/software: When using OSPI as a boot media, I cannot use the uEnv.txt loaded in OSPI. It always uses the default what should I do to use the uEnv.txt loaded in OSPI?
Part Number: TMUX1574
Tool/software:
Highlighting how RC loads impact our timing measurements:
The presence of resistive and capacitive loads influences how quickly muxes can switch signals and how accurately they handle high frequency signals. RC loads…
Overview:
In many applications the recommended Semitec 103AT-2 thermistor can be used, or a thermistor with the same specifications may be used. When the 103AT-2 is used or other thermistor with the same specifications, the temperature ranges in the…
Other Parts Discussed in Thread: TCA6424A FAQ: Logic and Voltage Translation > IxC >> What is the Auto Increment Feature in I2C IO Expanders?
The auto-increment feature of I2C IO Expanders is when the registers of the device automatically increment…
Part Number: DRV8714-Q1 Other Parts Discussed in Thread: DRV8718-Q1 Tool/software: Gate driver (e.g DRV8714-Q1) has VDS over current protection. One of common debug work of gate driver is false VDS over current fault. Even if motor current is not high…
Other Parts Discussed in Thread: TCA39306 FAQ: Logic and Voltage Translation > IxC >> What is PassFET Hangtime?
To understand what passFET hangtime is, we need to define what a passFET is.
A passFET is a transistor where the drain and source terminals…
Part Number: TCAN1057A-Q1 Tool/software: Hello experts!
I have a question about the purpose of the Mosfet and diode in CAN interface? Further,How does CAN implement arbitration and error correction functions through hardware?