Part Number: 2N7001T-Q1 Other Parts Discussed in Thread: 2N7001T Hi Team,
Is there an alternative source you would recommend to the 2N7001TQDCKRQ1 to second source ourselves from a TI perspective? Device would need to be pin-to-pin, but does not have…
Part Number: 2N7001T-Q1 Tool/software: In my application VCCA = 3.3V and VCCB = 1.8V. Should I use the Ioh and Iol specification for 8mA to determine the min and max voltage output?
The 2N7001T-Q1 datasheet shows Voh and Vol for the different mA loads…
Part Number: SN74LVC1G126-Q1 Other Parts Discussed in Thread: 2N7001T-Q1 , SN74LVC125A-Q1 , SN74LVC2G125-Q1 Dear logic friends,
Harman has challenges with the speed of a buffer.
Harman is down converting from 3.3V level to 1.8V level at 73MHz
Before…
Hi Mythili,
The TXS0101-Q1 will not be able to buffer your signals as its DC drive strength is limited. Consider fixed direction translators, such as TXU0101, 2N7001T, or SN74AVC1T45 instead.
Regards,
Jack
FAQ: Logic and Voltage Translation > Voltage Translators >> Current FAQ
Here are the voltage level translation device recommendations for various industry standard interfaces:
Interface
Recommended Device
3.6V Maximum
5.5V Maximum…
Part Number: CD74HC4040 Other Parts Discussed in Thread: TXU0101 , 2N7001T
At present, the project needs to test the 26MHz CLK signal. There are the following issues with manual environment testing. Please help analyze and confirm. Thank you! 1. Can…
The DIN input of the TCA5405 must never float. So with this two-transistor level converter, you always need a pull-down resistor.
The TCA5405 activates when it detects a high-to-low edge at its input. (So the idle state should be high.) If the 1.8 V…
Part Number: SN74AUP1T34-Q1 Other Parts Discussed in Thread: 2N7001T , SN74AXC1T45 in datasheet, there is only introduction about the application of signal from low voltage to high voltage. please tell if it support the voltage reduction case.
Quickly find solutions to common questions about voltage translation (level shifter) devices by clicking this link. This FAQ answers the most common questions asked about these devices …… ……… …
Auto-Bidirectional Level-Shifters
Fixed DIR / DIR…