Other Parts Discussed in Thread: ACF2101 Hi!
I want to use ACF2101 as a photodiode amplifier.
I connect the ACF2101 as in typical connection on Fig 1a in datasheet, photodiode connected only to one channel. I am not using select switch, the supply voltage…
Other Parts Discussed in Thread: ACF2101 The ACF2101 dual switched integrator has one internal capacitor per integrator.
The internal capacitors are specced at 100pF, 2% with a tempco of -25 +/-25 ppm/°C.
Is there any matching data available for these…
Other Parts Discussed in Thread: ACF2101 Hi,
one of my customer wants to apply offset voltage 0 to 5V to com pin in ACF2101
what is the input range of positive input of op amp?
Also, do we have any application note for layout guide?
Thanks and Regards…
John,
You've asked many thought provoking questions that gave me some sleepless hours last night. Be aware that I'm now retired and thus have the privilege of offering opinions and guesses without validation or guilt. :-) So here are some opinions…
Other Parts Discussed in Thread: ACF2101 Hi there,
I hope someone can help me. I'm running some simulations with TINA using the SPICE model for the ACF2101 switched Integrator from the TI website. So far I've been able to get the circuit to integrate…
Part Number: TPS61390 Other Parts Discussed in Thread: ACF2101
The TPS61390 has built in current mirrors. You can select between two current mirrors, sample the voltage at a resistor connected to the mirror at a moment in time, and read back this voltage…
Other Parts Discussed in Thread: ACF2101 , IVC102 Hi All:
I am working with a design that uses the IVC102 but I need to add a null offset to the input to zero the detector offset out. The IVC102 does not have an input that I can use on that chip but the…
Hello,
I have implemented the programmable voltage to current converter that appears in Fig 10 of the spec sheet. In the output, however, I am not using SELECT (but the unswitched output) and I am going to a current feedback based inverter with a gain…
Other Parts Discussed in Thread: ACF2101 , LM741 Hi there,
I am having some problems getting the ACF2101 switched integrator to integrate. I've tried my best to troubleshoot but couldn't figure it out and am hoping that someone here can point out my…
Other Parts Discussed in Thread: ACF2101 Greetings,
I have some ACF2101 integrators in hand. They are said to have the noise level of about 10 mico-Vrms. But I don't know at what frequency would this noise value apply. Could someone help to tell me the…