Other Parts Discussed in Thread: ADS1610 , ADS1675 Hi ppl,
Can some1 suggest an ADC with the following features :
1 . It should have two channels
2. Minimum Sampling rate of 10MHz
3. Resolution 24 bits. Input signal will vary from -2V to 2 V.
4. Both the…
Other Parts Discussed in Thread: ADS1610 I have been searching for A/Ds for a new project I am working with and I have found what to me seems to be a hole in the product line for High Speed A/Ds. I need a device that can run in the 10 - 40 Mhz sampling…
Other Parts Discussed in Thread: PCM4220 Hi!
Can you tell me, why a high-speed precision ADC, like ADS1610 , couldn't be used with an additional noise shaping, in order to create a nice audio ADC?
This converter's output features 16-bit with still almost…
Hi Chuck
The signal that I am sampling has a carrier frequency anywhere from 200 kHz to 450 kHz. The sample rate is four time the carrier, so from 800 kHz to 1.8 MHz. I am using a board with a ADS1610 Sigma delta converter. The other option that I am…
Other Parts Discussed in Thread: ADS1610 Hi All,
I am using a system composed of C6747 (300 MHz floating) and TI's ADS1610 (ADC, 10 MSPS). The 16 bit ADC output is directly conected to the GPIO bank 0 (GP0[0:15]). Data Ready of the ADC is triggering through…
Other Parts Discussed in Thread: ADS1610 , MSP430F2410 We are planning to interface a 16-bit, 10 MSPS ADC (ADS1610) with the MSP430F2410. Are there going to be any issues reading data into the MSP430F2410 every 100ns?
Hello Mitja,
Apart from the on board ADC, i dont think it would meet my conditions,for this purpose i am planning to use ADS1610 adc which has 16 bit res ,10msps, or ADS1278 with 24bit and 144ksps, and i think this sampling rate would be comfortable.…