Part Number: ADS41B49EVM Other Parts Discussed in Thread: ADS41B49 , Hello,
I am interested in evaluating ADS41B49 for a single ended input signal.
From the eval board datasheet it seems it can only accept differential inputs, is there any way to use single…
Part Number: THS4541 Other Parts Discussed in Thread: ADS41B49 ,
Hi,
I am currently testing a THS4541 to drive the input of the ADS41B49 ADC.
The input is DC coupled and I am using the recommended circuit specified in the THS4541 datasheet (Figure 80…
Hi Shinichi
Here is my suggested configuration for the customer. I highly recommend using ADS41B49 (buffered inputs) instead of the ADS4149 (unbuffered inputs). The unbuffered inputs of the ADS4149 will inject sampling noise back to the driving circuitry…
Hi David,
I don't think the ADS41B49 and ADC34J45 have the same equivalent input circuit. It looks like the ADS41B49 has differential input impedance of 10k||3.5pF at dc, whereas the ADC34J45 has a differential input impedance of 6.5k||5.2pF at dc. I…
Other Parts Discussed in Thread: ADS41B49 , ADS4149 What is the status of the clock outputs when in global power down or standby?
What is the power consumption when only the output is disabled?
Does global power down and standby disable the internal clock…
Other Parts Discussed in Thread: ADS41B49 , ADS62P49 , ADS5483 Hi,
Is there any reason I shouldn't use a source impedance of several hundred ohms with a TI ADC?
The TI datasheets typically show ADCs being driven from a 50ohm or 100ohm source, but the…
ADS41B49_serial_SPI_Test.pptx Jacob,
Take a look at the attached file. My ramp is going in the opposite direction. Not sure why the two are different.
Regards,
Jim
Hi All,
I want to design a WiFi operated Smart LED Bulb with Standard AC input and Also need to control dimming via micro controller as well as will drive WiFi module also.
Can anyone suggest me any solution for these requirement.
Can you suggest me IC…