Part Number: ADS5484 Hi,
I am using ADS5484 in my design.
When I am checking ADC output without giving any input, all the 16 bits are toggling.
I checked ADC power supplies. ADC power supplies are proper. ADC DRY is also coming.
Thanks in adv…
Part Number: ADS5484 Hi expert, I want to know the Data output frequency/Data output rate for ADC-ADS5484. Also i want to know the maximum length that we can route the input as well as output data signals.
Best Regards,
Part Number: ADS5484 Other Parts Discussed in Thread: ADS5485 , ADS42LB69
Hi,
My customer is considering using ADS5484.
However the datasheet of ADS5485 says that "ADS5485 is Not Recommended for New Designs".
Does TI recommend using ADS5484? …
Part Number: ADS5484 Hi,
Is latency of pipeline ADC fixed value? It is described in the spec column as TYP5 cycle. On the other hand, it is described in the explanation as 4.5 cycles on both edges. I believe this parameter is a value determined by the…
Hi Thinh,
Have you had further success with the evaluation? I have not been able to make substantial progress on my side, and, due to limited bandwidth on my end, will need to close this thread. Unfortunately, this EVM is quite old, and the original…
Part Number: TSW1400EVM Other Parts Discussed in Thread: ADS5484 , ADS5484EVM , ADS5281EVM Hi there,
Could anyone please give me an instruction (step by step including connection) about how to test a TSW1400 EVM with an ADS5484 EVM?
Much appreciate…
Hi Shivakant,
We have several options that will meet all of your requirements, except for decimation. Some examples are: ADS42LB69, ADC16DV160 and ADS5484.
Best Regards,
Dan
Other Parts Discussed in Thread: ADS5484EVM , ADS5484 Hi,
We are working on a project that uses the TSW1400EVM and ADS5484EVM, external clock, and external signal.
For the signal we are using 1MHz, and 1 V peak-peak
For the external clock we are…