Other Parts Discussed in Thread: SN74LVC2T45 , ADS8361 , ADS7861 , ADC122S625 , ADS7250 , ADS7251 , ADS7253 , ADS7254 Dear Community,
I'm looking for a dual channel 12-bit ADC (around 200Ksps) with 5V analog interface and 3.3V digital SPI (or I2C) interf…
Other Parts Discussed in Thread: ADS7861 The ADS7861 wery easy to damaged How to protect?
I use ADS7861 to decode SIN/CON encoder (with PMSM motor driver 15KW power). The ADS7861 work on mode #3 Before enable PWM Signal (IGBT control signal) The ADS7861 …
hi Tom : I can not reset ads7863 becourse I ues it to replace orginal device ads7861 (SDI =0) , are threre any more detal data sheet of ads7863 internal control logic structure? another problem I test ads7861 (CONV shorted with RD CS=0 m0=1m1=0 A=0) Busy…
Hi Yuri,
I have no SPI examples for the Raspberry Pi, however, there are several code snippets available for the ADS8361 and ADS7861 on various TI processors here: http://www.ti.com/product/ads8361#doctype1
The ADS8361 and ADS7861 are early version of the…
Hi Pablo,
Welcome to the forum! The peak soldering temperature is listed in the package addendum at the end of the ADS7861 data sheet (page 23). We'll track down the appropriate Theta J numbers for you.
Hi Victor,
See the following parts:
Part Number
Description
Resolution (Bits)
Sample Rate (max) (SPS)
# Input Channels
Multi-Channel Configuration
Input Range (Min) (V)
Input Range (Max) (V)
Interface
Integrated Features
Analog Voltage…
Other Parts Discussed in Thread: ADS7861 , ADS1251 , OMAPL138 Hello,
I want to generate a driver for the ADS7861 but I cannot find a Data Converter Plug-in Tool for CCS4. Can anyone help?
Thanks in advance,
Cor
Hi again Sanjay,
If I remember correctly, you are connecting the ADS7863 to the OMAP-L137. I'm not sure how well this will work using DMA, but the ADS7863 needs an active high signal applied to both the RD and CONVST inputs. There are several application…