Part Number: ADS8318 Other Parts Discussed in Thread: ADS8319 Hi,
On page 19 from ADS8318 , Figure 56 does not match with highlighted sentence as shown.
It should be as shown in Figure 45 from AD7687 which stated as cross-reference part for ADS8318. …
Part Number: ADS8318 Hi
as per one of the PCN#20191010001.1, lead finish is getting changed from NiPdAu to Matte Tin.
One of the part being used by us is affected bt this notice.
Part number : ADS8318IBDGST
1) Please let us know wheather,Nickel-layer…
Part Number: ADS8318 would you please advise ECCN for ADS8318? and are all this series the same ECCN, such as ADS8318IDGST? Thank you very much for the help!
Part Number: ADS8318 hello,
I have query on IC ADS8318. This IC has two power supply pins for analog and digital power supply and only one DEVICE GROUND pin which is common for analog and digital power supply, as per datasheet(refer page number 7). But…
Part Number: ADS8318 Greetings,
We have Technical Query on ADS8318IBDGS. which is considered in one of our design and we need the data urgently to support the design requirement.
Query: a. As per datasheet: Max Tj = 150°C & operating temp range (-40 to…
Part Number: ADS8318 What is the reference to the operating free air temperature range? Is it the air around the IC / board or is it the case temperature, or is it the junction temperature.
thanks,
-John
Other Parts Discussed in Thread: ADS8318 What is the output behavior of the ADS8318 is over the range and over the +Va? Specifically In+ and In- goes over or under the input range and exceeds the supply lines.
there are times our Op Amps will drive to…
Other Parts Discussed in Thread: ADS8318 , LP5907 Hi There - I'd like to understand if it would be acceptable to supply the +VA pin of the ADS8318 from say a LP5907 with a fixed 4.5V output. 4.5V is the minimum recommended supply in the datasheet (obviously…
Other Parts Discussed in Thread: ADS8318 Hi,
I am using ADS8318 as ADC IC, in the datasheet, it lits one way convert bipolar single-ended to unipolar differential. But I doubt it, I think the part in the red circule lacks connection between output and…