Part Number: AFE882H1
Hi TI Team,
I am working on HART physical layer conformance testing and have a question regarding LCD (Loss of Carrier Detect) error detection .
As per the HART specification, an LCD err should be generated when the Carrier…
Part Number: AFE882H1 Hi,
For AFE882H1, when CS pin is pulled down, AFE chip do not respond. When used while SPI communication, AFE chip responds. What could be reason? Pull down value 10k resistor.
Regards, Anurag
Part Number: AFE882H1 Hi,
Can we configure AFE882H1 chip with UART only.
We dont have to use SPI.
It is recommended to use only UART mode?
Do this have some limitations?
Regards,
Anurag
Part Number: AFE882H1 Hi,
Datasheet mentioned: Low quiescent current: 180 µA (typical)
With no communication, we get 300uA current.
Can we put AFE chip to sleep through software. OR It(180uA/300uA) is what we can achieve lowest.
/Anurag
Part Number: AFE882H1 Hi,
We came across this Tx frequency. Can you please help to which register is associated with this. I can see, output sine wave smoothness is depends on this selection.
/A
Part Number: AFE882H1 Hi,
We are using circuit fro, AFE EVM. We are facing issue of rise time for both 1200Hz and 2200Hz. As per measurement done as per HART physical layer testing standard from FieldCom. We changed the C12 to 1uF so it should not get…
Part Number: AFE882H1 Other Parts Discussed in Thread: XTR305 , Hi,
We have to implement HART FSK only. We are trying to implement by
It is working fine.
While physical layer testing, we had to change the cap C12(EVM SLAU888 - MAY 2023) to 0.5uF…
Part Number: AFE782H1 Other Parts Discussed in Thread: AFE882H1 , DAC7760 , DAC8771 , XTR200 , XTR200EVM , AFE882H1EVM hi expert,
How to design a 4‑20mA circuit compatible with 4-wire and 2-wire configurations using AFE782H1 / AFE882H1? Only 2-wire…
Part Number: AFE882H1 Other Parts Discussed in Thread: AFE881H1 I am using the SPI protocol for the interface of the AFE882H1 IC with the microcontroller
Below are the configurations added during the initialization of the AFE881H1:
1.Software reset…