Part Number: CC3220SF-LAUNCHXL I want to covert a string to a unsigned 64bit using atoll(), but the coverted value is incorrect. For below examples, only string 3 is correct. The coverted value of string 1 and string has filled FF instead of 00.
uint64_t…
Part Number: CC3220SF-LAUNCHXL Tool/software: TI C/C++ Compiler Hello,
I have copied a project and modified the sources and linked libraries.
After a while I am stuck in a undefined symbol issue. According to the output atol, memmove and strncasecmp are…
Part Number: CC2541 I am working on a project. Using cc2541 with IAR Workbench. In which i am having string of 13 Characters and that string contains only digits. So i want to convert that string to long so i used atol function and for that i included…
Part Number: MSP-EXP432P401R Hello Everyone.
Does the XDS110 Debug Probe work with Atollic TrueSTUDIO v8.1.0?
In Keil uVision 5, this debugger shows up as a "TI XDS Debug Probe".
This XDS110 debug probe is on-board the TI MSP-EXP432P401R development…
Part Number: CC3100BOOST Other Parts Discussed in Thread: ATOLLIC , , CC3100 , CC31XXEMUBOOST , CC3100SDK I experienced 2 problems:
1. using VisualStudio 2015 a linker error LNK2019: reference to extern symbol __imp_vprintf (in 2 different functions: DEBUG_PRINT…
Part Number: TDA4VM We’re trying to convert a feature extraction network based on torchvision resnet18 defined as follows:
torch_model = models.resnet18(pretrained=True)
return_nodes = {'layer4': 'layer4'}
model = create_feature_extractor(torch_model…
Other Parts Discussed in Thread: UC3827-1 Alas, I have a fully working supply using the UC3827-1 (buck, current fed). But, I have some alarm circuits that detect faults, and must disable the supply. I was trying to use the SS pin to disable, but it did…
user6202586 said: If this is not a good way, let me know.
That's not a good way. I highly recommend you use a function from the RTS library. Please learn about ...
atoi
atol
atoll
strol
strtoul
stroll
strtoull
I'm sure one of these functions will…
Here's a good example. Today I did a clean & rebuild at the following optimization levels
This function has never had this issue before until just now. It's in the stdlib.h's atoll function. Here's the function call.
All good…