Part Number: BQ32002 We would like to use RTC, BQ32002 in our products. We also use a multiple-output clock generator, which can generate clock frequencies from 5 MHz to 200 MHz. The BQ32002 requires a crystal oscillator. I was wondering if I could use…
Part Number: BQ32002 Other Parts Discussed in Thread: MSP430F6779A , Hi Team,
Good wishes to you. I'm working on RTC BQ32002 in my custom board(Using Microcontroller MSP430F6779A).I need to read RTCBQ32002 from micro controller MSP430F6779A Seconds and…
Part Number: BQ32002 Do we need to add external capacitors to 32.768Khz crystal?
Does the BQ32002 has internal capacitors close to 25pF (as Crystal load capacitance is 12pF requirement)?
Thanks, Darshan
Part Number: BQ32002 HI,
Two questions:
Q1: what does Vback at "Operating" and "Switchover" mean? if Vback <1.4V, the BQ32002 will be shut down and no any time counting, right?
Q2: What is relationship between Vback at "Switchover…
Part Number: BQ32002 Hi Team,
Do we have P2P solution with M41ST87WSS6F or function like suggestion?
https://www.mouser.tw/ProductDetail/STMicroelectronics/M41ST87WSS6F?qs=533gYOQZ5gSwTK1lfVjhxA%3D%3D
Best regards,
Hardy
Part Number: BQ32002 Hi CTS Apps,
I am curious if the BQ3200x can be used without the IRQ pin functionality. My customer is just looking for a basic RTC and I do not know if the Processor will have enough IOs to accommodate the IRQ. Can we go without…
Part Number: BQ32002 Hello,
My customer wants to know the reflow condition of the BQ32002DR.
Could you please provide a recommended reflow profile for the BQ32002DR?
Thank you.
JH
Part Number: BQ32002 Hello,
My customer has BQ32002 failure issue during system production.
Could you please review the customer circuit below for any issues?
Thanks a lot.
JH