Part Number: BQ32002 Hello,
My customer wants to know the reflow condition of the BQ32002DR.
Could you please provide a recommended reflow profile for the BQ32002DR?
Thank you.
JH
Part Number: BQ32002 Hello,
My customer has BQ32002 failure issue during system production.
Could you please review the customer circuit below for any issues?
Thanks a lot.
JH
Part Number: BQ32002 Hi team!
I am looking into a solution to make a real-time clock on a design I am working on really accurate. I am working on a sound level meter that needs to have accurate timing in order to report accurate numbers to our users. We…
Part Number: BQ32002 Other Parts Discussed in Thread: BQ32000 , BQ32KSW-LINUX Hi,
I would like to know if a Linux Driver for the BQ32002 is available. The driver below appears to be for the BQ32000, will it also work for the BQ32002?
BQ32KSW-LINUX( )
Best…
Part Number: BQ32002 Hello,
1. Please review the BQ32002 circuit below.
2. The specifications of Y1 are as follows.
Do I need C555 and C556 capacitors? If so, how should I calculate the values?
Thanks in advance.
Regards,
JH
Part Number: BQ32002 Hi team,
My customer is evaluating our RTC to replace intersil's ISL12057.
There are two questions and would like to consult with you.
Whether they need to change crystal part with 12pF load capacitance if use BQ32002DR? The…
Part Number: BQ32002 Hello,
Is there a range of crystal resonant frequencies allowed by the BQ32002?
What is the tolerance MIN/MAX ?
Thank you.
Regards,
JH
Part Number: BQ32002 Hello,
Can I use a crystal with load capacitance of 9pF for the BQ32002 RTC. In the datasheet under Recommended Operating Conditions, 12 pF nominal is recommended.
Thanks and Regards,
Arun M
Part Number: BQ32002 Hello TI experts,
I asked about the weird operation of BQ32002 ;
https://e2e.ti.com/support/clock-and-timing/f/clock-timing-forum/970909/bq32002-clock-information-reset-when-the-system-is-reset/3593851?tisearch=e2e-sitesearch&keymatch…
Part Number: BQ32002 Hello team,
We are using the RTC in a application where there is No need to remain clock while the device is powered off and it will be time synchronized by the system master clock when device start again. So can I keep the Vback pin…