Part Number: AM5749 Hi team,
Related to below post, there is an additional question from the customer.
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1013366/am5749-emif2-unused-pins
As discussed on the datasheet, the connections…
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5146-Q1 Hi,
My customer designs DCDC with LM5164-Q1. However, after staring FANs, LM5164-Q1 stopped SW output for 1 - 2 seconds. WHY does this phenomena occur? Please let us know how to resolve…
Part Number: TPS62090 When the output waveform of SW pin (1 / 2pin) was confirmed, the Low side was It was about -0.4V, which exceeded the absolute maximum rating of -0.3V.
Could you tell us about the following two points?
1. Since it is an absolute rating…
Part Number: ADS1299EEGFE-PDK Other Parts Discussed in Thread: ADS1299
Hi TI's expert,
I downloaded the ADS1299EEGFE-PDK-SW and used the ADS1299EEGFE-PDK boad to test the RLD function, everything works well except that when I wanna enable the Bias…
Part Number: AM62A7-Q1 Tool/software: Hi TI experts,
We have encountered a problem. After image is displayed, the screen occasionally flickers.
The video pipeline as below:
We captured the video when issue occurred as below:
mmexport1720095533897.z…
Hi Lei,
here are the requested measurements:
Note: At the right-hand end of the illustrations, where the temperature decreases rapidly, you can see the shutdown of our product.
Figure 1 (above) shows:
the temperature curve of the regulator, measured…
Hi, Daolin
Thanks you replies, let's me make some updates.
Steps as below,
a) Test Environment :
iperf3 server : 192.168.10.99
iperf3 DUT : 192.168.10.3
DUT OS : regular Linux without RT
b) DUT threads after boots :
PID USER VSZ STAT COMMAND…