Part Number: TPS65133 Other Parts Discussed in Thread: BUF602 ,
Dear TI experts,
I'm designing a system using the TPS65133 to power a high speed op amp (BUF602).
In my application, Vi comes from 3.7V from a 350mah Lithium battery.
Currently, I ha…
Oh and I saw there was a new version of the BUF602, the BUF802 JFET input 3GHz unity gain buffer, also +/-5V capable,
There might be a bit too much going on inside this for your needs vs the simpler BUF602,
Other Parts Discussed in Thread: BUF602 I want to send a 10 MHz clock signal for 300 ft from a modem to a Transceiver over 75 ohm coaxial cable.
Can you recommend a low cost solution with drivers and receiver, with perhaps some pre-emphasis/conditioning…
Well Certainly Archie, you can drive them with anything you want just treating the input as wideband Buffers (kind of like the BUF602's). We even supported AC coupled if need be adding an on chip mid supply reference buffer you would use on the input…
Hi, I am currently locked out of PSPICE (apparently too many installs, even though I uninstalled the only copy I actually had installed in order to reinstall it). Therefore, my simulation is currently in another simulation tool. That probably doesn't help…
Other Parts Discussed in Thread: BUF602 , OPA615 , OPA860 , OPA356 , TINA-TI Hello,
I need a high speed peak detector which can detect surge voltage however rising time of my voltage is approximately 0.7 ns.I read the TI forum note with OPA615 and BUF602 yet…
why don't you use the BUF602 if you want a single 5V buffer.
The Buf634A has an output headroom of about 2V on each side, on 5V supply - probably not going to work physically much less the model