Part Number: BUF634 Hi Sir
My customer application as below and need V+ is 15V/V- is -15V.
8th BPF
Input 25KHZ square wave 3.3V
Filter BW 2KHz
The output waveform is sinewave. Phase 0 degree.
Are BUF634A suit this kind 8th BPF application? or are there…
Part Number: BUF634
A1/A2/A3 is three control loops, A3 is the innermost loop, its bandwidth is 20MHZ, A2 is the penultimate loop, so according to the datasheet, I think its bandwidth should be within 20MHZ/4=5MHZ. Hypothesis: R2 = 100k and C2 = 10pF…
Part Number: BUF634 Other Parts Discussed in Thread: OPA659 , Hello team,
Hope you are doing well. I have a customer looking for an buffer equivalent for LH0033J. From what I see on TI.com I recommended OPA633 / OPA659.
However, the customer needs surface…
Hi,
1. Section 9.4.1.3 of the datasheet, Table 6, has recommended resistor values for each gain setting. These resistor values are selected to try to achieve the best noise performance, harmonic distortion, and for any noise gain peaking. All device…
Part Number: LMH6321 Other Parts Discussed in Thread: BUF634 , , TINA-TI , OPA593 , OPA593EVM Hi,
does TI offer a full simulation model of the LMH6321 chip? The downloadable SPICE files from TI explicitly state "* MODEL DOES NOT HAVE PROGRAMMABLE CURRENT…
Part Number: BUF634 Other Parts Discussed in Thread: LM6171 For an older headphone amp I need a new design of railsplitter / pseudo-ground-driver
Now I found a hint in BUF634 datasheet. My question, how much could be the value of the both cups C (1) on…
Part Number: ADS1258-EP Other Parts Discussed in Thread: ADS1258 , REF2025 , BUF634
Hello,
1. We want to measure 16 sensors single ended with the ADS1258. The sensors are configured as a quarter bridge with the circuit taken from the TI example below. R10…
Part Number: OPA2890 Other Parts Discussed in Thread: BUF634
I Designed with this circuit by TI Filter design, with OPA 2890.
The 4.2 kHz filtering circuit ran as intended.
But when I only change the center frequency 4.2 to 5.5 kHz,
It has…