Part Number: AM6442 Other Parts Discussed in Thread: AM6422 , TMDS64EVM
With same configuration and same board, the icssg0 two MII ports don't work with SDK9.1, it can detect PHY link, but can't ping through. the same board can work with SDK8.6…
Hi Lucas,
Correct. AUX is used to power the chip. The TPS25810 uses the CC lines to detect a load. The CC lines look for an Rd presented to know when a load is connected.
The TPS25810 has two pins, CC1 and CC2 that serve to detect an attachment to the…
dear nikhil:
yes,the DP83TC811 driver(new kernel) of read/write interfaces had working in the 3.18.120 Kernel after we modify :
change phy_write_mmd to phy_write_mmd_indirect
and change phy_read_mmd to phy_read_mmd_indirect.
My test steps: ifconfig eth0…
Hi ,
The DP_IN and DM_IN of the TPS25831 is mainly used for DCP auto charging function which have including the apple divider 3 (2.4A) mode and Samsung mode .If you focus on data communication you better chose TPS25830-Q1 or you can choose 831 but don…
Other Parts Discussed in Thread: CC2543 , CC2543-BROADCASTER-RD , CC2540 Dear TI Folks,
May i check with you do you guys have any additional information such as test report or profile on power consumption for CC2543 application? My customer is especially…
Part Number: PHYTC-3P-PHYCORE-AM335X Hello,
We have two devices based on PHYCORE-AM335X and are using Ti Linux kernel V4.4.62 on one and V5.10.65 on other.
We have a software application to create and write CSV file on USB devices using fopen,fread,fwrite…
Hi Ky,
You can take a look at the SW available at the bottom of this page: www.ti.com/.../TIDC-MINI-BLUETOOTH-LOW-ENERGY-BROADCASTER
It is for the CC2543, but it will be quite similar for CC2541.
Cheers,
Fredrik
Part Number: CC2650EM-5XD-RD Other Parts Discussed in Thread: CC2650 Tool/software: Code Composer Studio Can someone help me deploy the simpleperipheral for CC2650EM_5XD?
Steps I have done
1. imported simple_peripheral_cc2650em into the workspace
2.Changed…
for mmc dev 0
=> mmc dev 0
switch to partitions #0, OK
mmc0(part 0) is current device
=> mmc info
Device: mmc@fa10000
Manufacturer ID: 70
OEM: 100
Name: IB291
Bus Speed: 200000000
Mode: HS200 (200MHz)
Rd Block Len: 512
MMC version 5.1
High…
Hi Ferdinand,
The Mini BLE Broadcaster reference design is discontinued. For a small form factor reference design for the CC2541 you can look at: www.ti.com/.../CC2541-POSTAGE-STAMP-RD
Regards,
Fredrik