Part Number: CDCE913 Hi team,
Is it not necessary to connect to I2C when using this device in its default configuration? If not, please tell me about the pin handling.
Sincerely. Ryu
Part Number: TMDXIDK5718 Other Parts Discussed in Thread: CDCE913 , hello
I have a question about the TMDXIDK5718 evaluation board.
18pF is mounted on the load capacitors C172 and C173 of the crystal unit of U23 (CDCE913).
Is this 18pF because the register…
Hi Team,
The customer has a input signal which is based on 3.3V logic, however the CDCE913 accepts only 1.8V swing at input clock. Could you suggest the best way to convert the input swing of source 0 - 3.3V to 0 - 1.8V to give the input to cdce913
Part Number: CDCE913 Other Parts Discussed in Thread: CDCE6214 Hello TI experts,
My customer considers CDCE913 for their new product now.
the problem is, they use 3.3V input and output, and they only have 3.3V power rails,
But CDCE913 needs 1.8V for Vdd…
Part Number: CDCE913-Q1 Other Parts Discussed in Thread: CDCE913 , CDCEL913-Q1 Hi team,
What is the difference between CDCE913-Q1 and non-Q1?
From the datasheet, I’ve found below listed is different:
Operational temperature
Thermal parameter
…
Part Number: CDCE913 Other Parts Discussed in Thread: TDC1000 , TDC7200 , CC2538 , BQ25570 , Hello,
I am designing a board using these components from Texas Instruments,
TDC1000
TDC7200
CC2538
BQ25570
CDCE913
I will use BQ25570 to supply 3V to rest of the…
Part Number: CDCE913 Hello,
I am designing a system to generate MCLK for audio converters from external word clock (LRCLK). Your application note looks perfect for what I need but I need to support many word clock rates from 44.1k to 192k. I see in the…
Part Number: CDCE913 Hello Team,
I have a very technical query relayed from my customer about how increasing and decreasing output frequency is done on this device. Please see the full description of customer's case below:
I have a certain video scaler…
Part Number: CDCE913 Other Parts Discussed in Thread: CLOCKPRO hi ti team
How to config CDCE913 register to work with DS90UB941AS?
For example my video timing is 4096*781*60 and using 27M External Crystal.