Part Number: CDCM9102 Hi team,
Can we provide a high resolution schematic of CDCM9102 EVM. The picture quality in the EVM user guide is not so good.
Thanks a lot!
Yangbo
Part Number: CDCM9102 Hi,
I have questions about CDCM9102. My customer are planning to use CDCM9102 as PCIe clock generator. They have following questions:
Q1. Does CDCM9102 support external oscillator input(3.3V)? Or does it only support crystal input? If…
Part Number: CDCM9102 Other Parts Discussed in Thread: CDCE62005 Hello,
The CDCM61004 has a temperature drift limitation of 100°C (indicated in datasheet since revision H January 2016).
The CDCM9102 which is a "similar" device does not exhibit such…
Part Number: CDCM9102 Other Parts Discussed in Thread: CDCLVC1104 , CDCLVC1103 Hello.
Can I input a clock that is not a crystal to CDCM9102? I would like to input the 25MHz output of CDCLVC1104 or CDCLVC1103 to the XIN terminal of the CDCM9102. Is it possible…
Hi,
Kindly use the crystal with load capacitance 10pF and shunt capacitance 7pF. In summary this device is very sensitive to crystal characteristics. We faced the same problem with18pf load capacitance crystals. Later as per the cdcm9102 data sheet…
Part Number: CDCM9102 there is recommendation of input crystal of CDCM9102 in d/s, how to select it? whether there is some spec need about crystal?
many thanks
Part Number: CDCM9102 I have a customer who is targeting the CDCM9102 for a PCI Express application. Can someone respond to the 3 questions below?
1. Datasheet says that it is a low-jitter clock generator designed to provide reference clocks for PCI Express…
Part Number: CDCM9102 Other Parts Discussed in Thread: AM5718 , Tool/software: Linux Hi,
We have designed single board computer with AM5718. We have PCIe based ethernet peripheral. For PCI we are using CDCM9102 Clock generator. The clock is coming from…