Part Number: DAC121S101QML-SP Hello,
For the 5962R0722602VZA (DAC121S101WGRLV), i was wondering whether the package contains floating Metal and if the lid of the device is grounded. Thanks!
Best,
Adam
Part Number: DAC121S101QML-SP Hi,
Can the 5962R07726, space rated version, share the clock(SCLK) and/or data(Din) lines for multiple devices? If so, what is the recommended number devices that can share the data and/or clock lines?
If the data and…
Part Number: DAC121S101QML-SP
What is the output impedance of DAC121S101QML-SP when in power-down mode or the part loses power?
I see that the DC output impedance is typically 8Ohm under ROC.
Part Number: DAC121S101QML-SP According to the datasheet:
"7.3.4 Power-On Reset The power-on reset circuit controls the output voltage during power-up. Upon application of power, the DAC register is filled with zeros and the output voltage is 0 V and…
Part Number: DAC121S101QML-SP HI team,may I ask Op Temp (°C) 25 to 25 for DAC121S101WGMPR (pg28) in the datasheet is correct?
www.ti.com.cn/.../dac121s101qml-sp.pdf
My customer want to know DAC121S101WGMPR & DAC121S101WGRLV
contains the same IC…
Part Number: DAC121S101QML-SPDAC121S101QML-SP: During power-on, I'm seeing a voltage transient on the DAC output. The transient is about 800mV and lasts about 2ms. The DAC supply voltage is ramping up from 0V to +2V during this time (on its way to final…