Part Number: DAC8551 Other Parts Discussed in Thread: DAC161S055 , , DAC8811 , DAC8811EVM , OPA277
Team,
We are trying to understand the device parameters that gives or influence the frequency of the output signal. Goal is to find out what is the maximum…
Part Number: DAC161S055 Other Parts Discussed in Thread: OPA544 , OPA548 I am using the DAC161S055 as a 0 to 5VDC source. I would like to increase the current drive to at least 3A with good 1:1 voltage following.
Part Number: EK-TM4C1294XL Other Parts Discussed in Thread: ADC161S626EVM
Hello,
My test application is basically takes the input of an analog signal (sine wave from the signal generator) convert it with the ADC161S626EVM BoosterPack and outputs the same…
Other Parts Discussed in Thread: DAC161S055 Hello I have the F5529 launch pad and the DAC161S055EVM booster pack. Is there any CCS based source code (or projects) that I can use to get jump start on development?
I attempted to load the LabView based firmware…
I'm transmitting a ramp via SPI to the board, but the output is sitting midrail.
I'm powering VA and VDD with 5V. J1 is connecting pins 2 and 3 to use the onboard regulator. and i'm connecting LDACB to ground on the test port.
over SPI i've…
Hi Garrett,
Thank you for your reply.
I have two new issues now and need your advice. As , I am working on SPI cimmunication between msp432p401r and dac161s055.
1) I used SPI master increment example from driver library to do communication between msp432…
Hi Chris,
Thank you for your brief explanation. I did in similar way but this approach was not efficient for my project. So, I decided to speed up SPI protocol. For that I have done almost all work but i am not understanding what will be my destination…
Hi Stefan,
I have done with ADC part with your help and it is working fine now. From last 2 days, I am trying to do SPI communication between DAC161s055evm and MSP432.
In dac161so55 data sheet page 16 , it is written that data can be sent from PREREG…
Part Number: MSP432P401R Hi,
As , I am working on SPI cimmunication between msp432p401r and dac161s055.I have two issues now and need your advice.
1) I used SPI master increment example from driver library to do communication between msp432 and dac161s055…
Good morning Chris,
As I am using floating point feature of MSP432P401R, I am using following values for above defined parameters:
filteredf_output are float values which are coming from the multiplication of filter coefficients and input.
AdcValueDigits…