Other Parts Discussed in Thread: DAC37J82EVM , DAC37J82 , DAC37J84EVM Hi,
I've successfully set up the eval board to generate a 20MHz signal using the following simple set up.
However, when I try to up the DAC rate to twice that value using the following…
Amy,
Please send the DAC GUI Quick start tab screen shot. Are they using the TI DAC37J82EVM? What is used to send data to the DAC? If it is the TSW14J56EVM, send screen shots of the HSDC Pro GUI and LED status of both boards. Make sure both boards have…
RajK,
This is incorrect. The output needs to be referenced to GND. See attached DAC37J82EVM schematic for reference.
Regards,
Jim
2235.DAC3XJ8XEVM-SCH_D.pdf
Part Number: LMK04828 Other Parts Discussed in Thread: DAC37J82EVM Hello, I'm running into an issue on the LMK04828 in which the SDCLK outputs don't invert their signals, regardless of their setting in the register map. I am using this part on a DAC37J82EVM…
Other Parts Discussed in Thread: DAC37J82EVM , DAC37J84 , LMK04828 Hello,
We were directed to you according to the following message: The part number cannot be recognized; it is this one DAC37J82EVM.
33395 points Kang Hsia
Jul 5, 2019 4:32 PM
…
Part Number: DAC37J82EVM Other Parts Discussed in Thread: DAC37J84 , LMK04828 Please find below our query which was originally issued in German language. The translation is done by a person with no technical background.
This question is subject to official…
Part Number: ADS54J20EVM Other Parts Discussed in Thread: DAC37J82EVM , ADS54J20 Hi ,
I'm using ADS54J20EVM and DAC37J82EVM interfaced with KCU105.
Kindly send me ADS54J20_LMF_8224.ini and DAC3XJ82_LMF_82X files.
Thanks
Jagadeesh
Other Parts Discussed in Thread: DAC37J82EVM I have used the TSW14J10EVM and Xilinx KC705 combination to test the DAC37J82EVM, so I know how the combination works.
However, I was told by Joshua Carnes that the ADC31JB68EVM will also work with the TSW14J10EVM…
I now have the ADC31JB68EVM, the DAC37J82EVM, the TSW14J10EVM, and the Xilinx KC705.
The DAC37J82EVM + TSW14J10EVM + KC705 combination works.
I use the DAC3XJ8X GUI to configure the DAC, and use the HSDC Pro to control the KC705 fpga carrier via the TSW14J10EVM…
DAC37J82_DAC_NCO_demo.pptx DAC37J82_NCO_50MHz_reg_settings.csv user4,
If you are using the TI DAC EVM with a TSW14J56EVM, you can follow the attached slide show to get this setup up and running. If this is a custom board, I have also loaded the register…