Part Number: TSW14J57EVM Other Parts Discussed in Thread: DAC38RF89 Seen several post regarding the TSW14J57EVM and DAC support. Over a year ago the post suggested that a new version of the board would be available to support DACs ... but I'm not seeing…
Lalit,
For query #1, you can achieve this rate if you use external DAC clock or switch to the DAC38RF89, which has a 5GHz VCO.
For query #2, the only options available are the ones shown in this table. Even though the part can have a serdes rate and sampling…
Toshihiro,
Attached are examples of both cases with the sample rate at 3200Msps and an output of 100MHz.
Regards,
Jim
41380_single_12_bit_real.pptx 82380_12_bit_single_real_1x.pptx
Part Number: DAC38RF82 Other Parts Discussed in Thread: DAC38RF89 hello,
We have a one JESD204B master implemented on a Xilinx FPGA (ULTRASCALE device).
In the FPGA configuration M=2, L=8 (LMFS).
Eight serdes lanes are connected to the DAC38RF82.
We have…
Part Number: LMK04828 Other Parts Discussed in Thread: LMK04832 , ADC12DJ3200 , DAC38RF89 Hello,
My customer has a question about LMK04828.
[Q]
Please tell me the variation (min and max) of the VOD for the following output level.
* LVDS
* LVPECL 1600mV…
Part Number: DAC38RF82 Other Parts Discussed in Thread: DAC38RF89 hi,
We have four DACs that we want to operate them at 2500MSPS input data rate and interpolation 2 (using DAC38RF89), or 3333MSPS input data rate and interpolation 2 (using DAC38RF82). …
Part Number: ADC12DJ3200 Other Parts Discussed in Thread: DAC38RF89 hi all,
we are observing a strange behaviour on a design involving DAC38RF89 and ADC12DJ3200.
We setup a system in such a way that only DAC and ADC are involved in the analog path.
…
Hi Rajesh,
Attached are slides to walk you through setting up the DAC in your desired mode. The LMF = 823 mode requires 2 clock sources to setup successfully.
Thanks,
Eben.
DAC38RF82_real_811_8_bit_mode.pptx
DAC38RF82_82380_12_bit_single_real_2x.…
Dear Jim
hi,
I saw TSW14J57 support assessment of DAC38RF89 on TI official website, so I bought TSW14J57, but found that it could not be evaluated, so I wanted to apply for TSW14J56, so the seller asked me to provide some evidence. Can you help me? …