Part Number: DAC7811 Hi team,
When only one device is used and the daisy chain is not required, does the command, "Daisy-chain disable" need to be sent?
Regards,
Noriyuki Takahashi
Part Number: DAC7811 We are using DAC7811 in a new design in daisy chain mode. 32 bits in one sequence.
There are certain data pattern that lead to "freezing" the DAC7811. After sending these pattern the DAC will not accept any further data. The output…
Hi Amy,
Thank you for your query. I don't see any problem in the waveform. The root cause of the problem might have to do with some miswiring or some power supply not coming properly to the devices. Could you please confirm all the connections and power…
Part Number: DAC7811 Other Parts Discussed in Thread: DAC8811 Hi team,
I am considering replacing another maker's multiplying DAC with DAC7811 at my customer. Please see the attached file.
DAC_circuit.xlsx I think that DAC7811 is usable and the Cf…
Kato-san,
The two devices are somewhat similar, the most significant difference I see in the datasheets is that the DAC8043U is rated only for operation from -40C to 85C while the DAC7811 is rated from -40C to 125C. However, both device electrical…
Part Number: DAC7811 I combind spartan3E with my DAC7811, when it comes to simulation, everything is ok, and when there are 17 periods of sclk in a period(One period in SYNC=1), it can output something.However, when I change the period to 25 (9 in SYNC…
Part Number: DAC7811 Other Parts Discussed in Thread: DAC8811 , DAC8822 , DAC8820 Hi, Experts:
May I have a question of the reference multiplying bandwidth for the multiplying DAC DAC7811.
As the digital codes goes smaller, the current going out…
Part Number: DAC7811 The DAC7811 datasheet refers to the ability to interrupt a command by de-asserting SYNC/ before the 16th falling edge of SCLK. Do I explicitly need to issue a "Daisy-Chain Disable" command before the SYNC Interrupt will work correctly…
Part Number: DAC7811EVM Other Parts Discussed in Thread: DAC7811
I am working on DAC7811 and spartan-3e fpga i want convert my digital data into analog value for that i make give three inputs to the DAC7811 from fpga board those inputs are mosi and…
Part Number: DAC7811EVM Other Parts Discussed in Thread: DAC7811 hello...
i
i am working on DAC7811 and spartan-3e fpga i want convert my digital data into analog value for that i make give three inputs to the DAC7811 from fpga board those inputs…