ADC_SAMP_INST sets the instance when ADC is sampled within each Pwm period.
So long as sinewave gen update is done from within an ISR, it should be independent of any non interrupt codes.
interrupt void reslvr_ISR ( void )
{
// RESTART_CLOCK_C28…
1.A customized board? Or TI EVM board? ->Either customized chips or development boards, or mass-produced chips
2.Which lab are you using? -> 12b
3.Any current current waveforms to show the issue? ->
1) 0741.user.h
Any settings in the user…
Dear all,
is there anyone who is using the same kit or similar ones?
I'm now using the function "sinewave" provided by TI to generate Sin PWM, I got two problems about that:
conditions: EPWM1_TIMER_TBPRD = 280; fc=107.14KHz, up-down count mode…
Hi Kiruba,
thank you for your interest in our device. Please find below the answer to your questions:
1) the jitter requirement for the ADC depends on the maximum analog input frequency which is sampled, the target SNR and the aperture jitter of…
spru714 datasheet.pdf TI RefDesign guideline.pdf DC-PLC Refernce Design.pdf Hi,
I am working on PLC, give me the solution for following requirements for PLC:
Carrier modulation: BPSK
Carrier Frequency:132KHz
Power Line Voltage:220VDC
Data Rate…
Daniel,
TI no longer supports the TSW14J56EVM as it is now obsolete. The firmware developed for this platform was done by a third party, which no longer supports TI. The board has a JTAG connector that will allow you to download your own custom firmware…
Chaithra,
I do not know much about the AFE5818, but no ADC is perfect and every capture will be slightly different due to the lower bits of the ADC toggling.
For your other questions, please see the attached HSDC Pro User's Guide.
Regards,
Jim…
Vaibhah,
1. The configuration file I sent programmed both the LMK and DAC to allow for this output. JESD data was not used so the JESD reset and sysref trigger are not required.
2) Also, as I am trying to increase the NCO frequency the noise on the…
Paven,
The results from the software can be displayed in either dBFs, dBc or Hertz. See sections 3.6.1.5 and 3.6 of the attached User's Guide for more info.
Regards,
Jim
HSDC Pro user guide - latest version.pdf