Hi Pavithran,
Apologies for the delay in response.
CLKOUT being 25 MHz is to be expected, by default it will output whatever XI input is. CLKOUT can be adjusted to different outputs in Register 0x0170.
Could I ask what the 125MHz is to be used for?
In…
Part Number: DP83867IR Other Parts Discussed in Thread: DP83865 ,
HI ,
In our previous design, we utilized the DP83865 PHY chip, which functioned effectively for our purposes.
However, we recently replaced it with the DP83867IR PHY chip as a one-to-one…
Part Number: DP83865 Other Parts Discussed in Thread: DP83869 Hi,
What is the maximum supported packet size for this part? We see intermittent CRC errors in the Rx datapath for larger sizes when a modest (well under 100ppm) clock frequency offset is applied…
Part Number: DP83865 Other Parts Discussed in Thread: DP83869 I need help finding a pin-to-pin replacement for the DP83865DVH/NOPB. Are there any alternates in the same package? This part is NRND and I'm trying to find another option.
Part Number: DP83865 Can you please confirm if this is a valid marking for this component? We've had a recent failure of new production boards and they all have this version of part which looks quite different from previous parts I've seen. The part number…
Part Number: DP83865 Other Parts Discussed in Thread: DP83869 Does the DP83865 support PTP/PPS?
I seem to recall that DP83865 supported PTP/PPS but now I do not see any mention of this in the datasheet. Was it de-featured?
-Matt
Part Number: DP83865 Other Parts Discussed in Thread: AM3352 Hello,
I'm using DP83865 on a custom board with AM3352 chip.
The PHY can be link up state in 100Mbps full duplex mode and transmit data.
But the data transmitted from the PHY misses some…
Part Number: PROCESSOR-SDK-J721E Other Parts Discussed in Thread: DP83865 MCAL Package: MCUSW_09_00_00_10_CONFIG + sdk-rtos-j721e-evm-09_00_00_02 The following Autosar APIs are not defined in ETHTRCV source Code:
EthTrcv_CheckWakeup (SWS_EthTrcv_00134) …
Part Number: DP83865 I have inherited a design built around this PHY. 10/100 communication operates great, but at 1000 at least half of our products start exhibiting buffer errors and fail to communicate. This design is several years old and this has…