Part Number: DRV135 Other Parts Discussed in Thread: DRV134 Hi,
Does the DRV134 have any restriction for power supply sequence?
Best Regards,
Kuramochi
Hi Kiran,
You can select one of our Line Drivers based on your application requirements.
If you need single-ended input and differential output, you can consider DRV134/DRV135. If you need differential input and single-ended output, you can consider DRV603…
Part Number: TPA2005D1 Other Parts Discussed in Thread: DRV135 , DRV134 , OPA2322 Hi,
I am using TPA2005D1 to drive my 8 ohm speaker, but it is producing audible pop and click sound whilst turning ON . How can we completely eliminate Pop and click noise…
Hi Pranav,
DRV135 should be able to drive a 30m cable. The typical application section (Section 9.2) of the DRV134/DRV135 datasheet shows an example circuit using a DRV134 to drive an INA137 through 500 feet (150 meters) of cable.
One question I have…
Part Number: DRV135 Other Parts Discussed in Thread: DRV134 , , OPA1678 , OPA1679 Hi TI,
Audio Codec L, R Output The DRV135UA (6dB AMP) is attached to each line to configure the circuit to perform Single Ended output.
On the datasheet, only DRV134 is shown…
Part Number: TLV320DAC32 Other Parts Discussed in Thread: TLV320ADC3101 , , DRV134 , INA134 Dear Support team,
May I ask about the recommended line driver for TLV320DAC32 and line receiver for TLV320ADC3101?
Does DRV134/5 match with DAC32?
Does INA134/7…
Hi David,
We have the DRV134 and DRV135 audio balanced line drivers, but I am not sure if their 100 kHz and the video performances are sufficient for the application. I suggest contacting the High-Speed Amplifiers group via their E2E forum. I expect that…
Other Parts Discussed in Thread: DRV134 , TINA-TI I downloaded DRV134 from ti.com
.
I can open DRV134 TİNA ti reference design as successively.Also,I downloaded DRV134 Spice model.Then I inserted DRV134 to my LT spice library. After that I built tina…
Part Number: TS5A22364 Other Parts Discussed in Thread: DRV134 HI Sir
1. if no signal connect with INx ,what's the default setting of TS5A22364 (NC to COM or NO to COM?)
2. When VCC=0V ,NC or NO pin can't supply negative voltage input ,Am i right…
Other Parts Discussed in Thread: TLV320DAC3120 , TLV320DAC3203 , DRV603 , DRV602 , DRV134 , DRV135 Hi TI,
There is an Audio requirement for one of my project where i get digital audio data through I2S interfacing from host processor and i need to convert it…