Part Number: TDA4VM-Q1 Hi,
I'm running camera through DS90UB962 using virtual channel.
I want change the format configuration but after setting, the DS90UB962 not update new format.
But both DS90UB953 and camera have been updated.
Here's the original format…
Part Number: DS90UB962-Q1 Hi TI team,
We have a request from the end customer is to convert the display data (HDMI 1.4, YCbCr422:24-bpp) to MIPI CSI(YUV422) output, the system block diagram is shown below, please help check if it can be achieved and whether…
Part Number: DS90UB962-Q1 Hi Team,
With a 953/962 pair, after Aliases are setup can you help me understand if both I2C channels can be used at the same time.
1a. For example can I2C1 be used to communicate back and forth to remote sensor1 while simultaneously…
Part Number: DS90UB962-Q1
Hi Team,
With a 962 when running in round robin forwarding mode, can you clarify how our RX line buffers confirm that a line is "ready for forwarding"?
The motivation for this question comes from my customer senario…
Part Number: DS90UB960-Q1 Hi there,
How would TI recommend issuing the same frame sync signal to several different DS90UB962 (or 960)?
We have the following schemes in mind:
In above block diagram, one of the DS90UB962 is generating an internal frame…
Part Number: DS90UB962-Q1 Hi Expert,
Our customer want to evaluate delay of 933+ 962. I search on e2e and find some related post. The main delay is caused by 962 video buffer. The max time is 2x line time due to video buffer. But there is only one video…
Part Number: DS90UB962-Q1 Hi Expert,
For the I2C master Proxy a below, from my understanding, this function allows real I2C master to access slave device on the Deserializer side, right? Then as for the real I2C master, I know it can be MCU located on…
Part Number: DS90UB962-Q1 Hi Team,
Cc: Justin Phan David Shumate
I have a few questions on the ub962 Register settings. Could you please clarify the below items?
Register 0x19, 0x1A, 0x1B, 0x1C (FS_HIGH_TIME & FS_LOW_TIME)
Currently our configuration…
Part Number: DS90UB962-Q1 Hi team.
My customer use 935/962 port3 and found 962 can't link when BC is 50Mbps, only can link when BC is 10Mbps. Below is the registers dump. Could you kindly tell me what is the possible reason? Thanks!
BR
Jiawei