Hi Vyom,
Vyom Mishra1 said: DS90UB964-Q1EVM
You are using UB964 whereas the driver has UB960 as default. Have you configured UB964 DES and integrated the same in sensor driver?
Vyom Mishra1 said: This camera is already bring-up with J721E with different…
Part Number: DS90UB964-Q1EVM Hi team,
Our customer is referring the EVM circuit, and they have a question with using the capacitor.
From the DS90UB96XEVM User's Guide , C84 is using 240pF on the EVM. Is there any concerned that change into 270pF, MLCC…
Dear Sir,
When I checked the same file(cslr_dss.h) present at the location
/psdkr/pdk_jacinto_08_02_00_21/packages/ti/csl/src/ip/dss/V4
Below are the values set
#define CSL_DSS_VIDL1_ATTRIBUTES_FORMAT_VAL_YUV422_NV12 (0x3CU)
#define CSL_DSS_VIDL1_ATTRIBUTES_FORMAT_VAL_YUV420_NV12…
Hi
We are using in our design DS90UB964, RIN0P RIN0N have AC coupling caps. PCB layout we should place the AC coupling caps near the 964 or near the FaKra connector.
some demo of 964 place the AC coupling caps near the FaKra connector,but the datasheet…
Part Number: DS90UB964-Q1EVM Other Parts Discussed in Thread: ALP Tool/software: Code Composer Studio ALP cannot recognize DS90UB964EVM (unknown device connect with DS90UB913)connecting the device with computer in USB cable.Then debugging programmer…
Part Number: TDA4VM-Q1 Other Parts Discussed in Thread: DS90UB913A-Q1 , DS90UB964-Q1EVM
Dear Sir,
I am working with
PSDK 08_02_00_05
Serializer: DS90UB913A-Q1 (ISX016)
Deserializer: DS90UB964-Q1EVM
Last Friday, we tested the application and it was working…
Part Number: DS90UB964-Q1EVM Other Parts Discussed in Thread: DS90UB964-Q1 , ALP Hello everyone:
I need drive the chip 913 and DB90ub964 through I2C by giving SCL and SDA generated by FPGA.While according to the paper" DS90UB964-Q1 Quad FPD-Link…
Part Number: DS90UB964-Q1EVM Other Parts Discussed in Thread: DS90UB913A-Q1 ,
Hi,
I am using 964evm and 913, and an image sensor.
There are CRC errors with the reg 0xc and 0xa of 913.
Can anyone help me with this?
Part Number: DS90UB964-Q1EVM Hello,
I got DS90UB964-Q1EVM and using LaunchPAD app to test the chip.
Currently I'm trying to run test pattern generation and BIST using the "Pattern Generation" or I2C via "Scripting" tab in app but i don't see any test running…