Hi,
My schematic review is as follows:
1. Please do the required gate resistance calculations to see if you will be able to drive your switching FETs. Too much gate resistance and you will not be able to switch the gates fast enough.
We could produce…
Part Number: TPS745-Q1 Hi TI engineers:
In our project, we use TPS74501-Q1 ,and for this chip we have a question for its “PG” PIN , in TI datasheet ,the typical application for PG should pull-up to Vout as you can see picture 1,we want to…
Hi Brandon!
Thank you for the suggestion. Yes, I added it to the PPHV as you earlier suggested. I was just wondering if VBUS is at 5V, then PPHV would also be at 5V. The Output of the LDO would then be less than 5V Maybe around 4.5V. I added TLV70245QDSERQ1…
Part Number: THVD8000 Hi ,
I am using THVD8000 Driver IC for my new project to power nodes from gateway device over two wire.
The scope of project is
1. Gateway can have maximum of 3 nodes and minimum of 1 node connected on Power over RS485 bus at any…
Part Number: FDC1004 Hi,
Need design review of the attached design.
/resized-image/__size/320x240/__key/communityserver-discussions-components-files/1023/pastedimage1674696395811v1.png
Here is the schematic interface:
/resized-image/__size/320x240…
Part Number: BQ24650 Hi team,
Could you review my design, please? See below the conditions and the file with the design.
Solar Panel 21V, battery Li-ion 1-cell, ICHARGE = 4 A, IPRECHARGE = 0.4 A
/cfs-file/__key/communityserver-discussions-components…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: TDA4VM Hello TI Team,
Could you please contact me for a design review of our TDA4VM board design based on the TDA4VM starter kit design PROC112E2 using the TPS65941213RWERQ1(PMIC-A) and TPS65941111RWERQ1…