Part Number: TPS546D24A Hi team,
I saw in a previous post that had a very similar issue to the one I am encountering:
"can you help give some suggestions when i use fusion digital power designer with TPS5436D24A on the project board but GUI shows "no…
Part Number: TLV3605 On the TLV3605, our design may have the analog power rail (VCCI, 5V) powered off for extended periods while the digital power rail (VCCO, 3.3V) remains powered. The comparator inputs (IN+, IN-) will be at ground as the whole analog…
Part Number: PCM2903 Hi!
I am using the PCM2903 ADC to digitize measurements. So my question is whether the digital output of the ADC is a digitalization of the Voltage (Volt) or the Power (Watt)?
Since these are not proportional: P = V*V / R
Part Number: TPS53622 Dears,
Regarding TPS53622, when modifying the firmware of TPS53622 with an input voltage range of 5V, it was found that VIN-ON and VIN_ UV values are not very friendly, VIN_ ON does not have a 5.0V modification option, but it has…
Part Number: UCD90160A Hello,
Is it possible to use USB-TO-ANY instead of USB-TO-GPIO to programm UCD90160A with Fusion Digital Power Design?
Thank you.
Best regards,
Kübra
Part Number: TPS546D24A hi team,
can you help give some suggestions when i use fusion digital power designer with TPS5436D24A on the project board but GUI shows "no device found"
USB TO GPIO LED is lighted, SCL/SDA/GND is connected, master MCU…
Hi Chris,
Sorry for the late answer.
I made the calibration above for all the rails and I have a good correlation between the load and the GUI.
I've tried it for an other board but the calibration were complitly different.
I suspect a board schematic…
Hi Expert,
I meet issue when installed below file 7.8.3,
4760.TI-Fusion-Digital-Power-Designer-7.8.3.zip
Issue:
but if i install 7.0.11 file, that will be fine.
TI-Fusion-Digital-Power-Designer-7.0.11.exe
Could you help to check what's the problem on…
Part Number: FUSION-DIGITAL-POWER-STUDIO Hello,
I have recently ordered UCD3138PSFBEVM kit and in that currently I have started working with UCD3138CC64EVM module independently. I had downloaded firmware of PSFB ( sluc614 ) from TI website and tried to download…
Part Number: FUSION-DIGITAL-POWER-STUDIO Other Parts Discussed in Thread: UCD3138 Hi ,
In UCD3138 Schematic. How to find value of R3,R4 and Cp2 ??
Could u please explain the circuit of Single phase Evm?/
Also ,the op-amp which is used in the circuit, Is…