Other Parts Discussed in Thread: INA159 The INA159 has a supply voltage range of +1.8V to +5.5V with an input voltage range of up to +17.5V. Does this mean that the amp could be powered by +5V and could be fed, say, a +12V input signal? The fixed gain…
Other Parts Discussed in Thread: INA159 HI All,
Is there anybody who can help provide me the parameters of ' Gain Long-Term Drift' or ‘Resistor Matching Ratio Long-Term Drift’' under condition of 70°C and 2000 hours for INA159? thanks in advance…
Hi Nima,
As I said, the ADS1256 cannot read signals below AGND directly.
Since you are showing a bipolar, single-ended +/-10V signal, you could use an INA159 to level shift as shown below instead of a resistor divider. Is this solution available to you…
Hi Jack,
Have a look at the INA159 - a Precision Gain of 0.2 Level Translation DIFFERENCE AMPLIFIER. It was designed to accommodate a (+/-) bipolar input voltage and convert it to a unipolar output voltage. It is usable with a single supply from +1.8…
Hi Nils,
The image below shows the INA159's output scheme given the connections you described (REF1 = GND, REF2 = VCC). I am not sure what VCC is on the waveshare board since this is not a TI product, but if it were 5V for example then the INA's output…
However, INA149 is a high common-mode difference amplifier with a gain of 1. This means that it is meant to be used for high-input common-mode voltages with the linear input differential signal being limited by the output voltage swing - see below. For…
Part Number: LM5025A Other Parts Discussed in Thread: INA159 Hi ,
My customer have used LM5025A for a long time, and TI design PMP4468 was exactly designed based on their requirement long time ago. their design closely followed this design and the BOM…
Other Parts Discussed in Thread: INA828 , ADS1248 , INA159 , ADS8688 , INA826 , ADS1262 Hi All
Ti have PLC A/D solution can be use same channel to sensor Voltage, AMP, RTD , Thermocouples (TC)?
This doc Tidu491 split 4 channel to do sensor , Voltage, AMP, RTD…
Part Number: INA821 Other Parts Discussed in Thread: INA338 , INA327 , INA326 , INA146 , INA137 , INA143 , INA159 , INA157 Hi Sir
Does TI have gain less than 1 IA solution
Which one is the latest ?
Thanks