Part Number: INA180-Q1 Hi Experts,
ZXCT1110QW5-7 is mass production in customer. Could you help to provide Pin-To-Pin device to replace ZXCT1110QW5-7? Thanks.
Best Regards
Songzhen Guo
Part Number: INA180-Q1 Hi,
Could you give the formula for getting current flowing through Rsense by output voltage of the current-sense amplifier.
I'm using INA180A2QDBVRQ1 in my design. In the data sheet it's mentioned the gain error factor and gain…
Part Number: INA180-Q1 Hi there,
Could you tell me Moisture Sensitivity Level (MSL) of the part INA180A1QDBVRQ1.
Thanks.
Best Regards,
Kaoutar Ben Kaddour
Part Number: INA180-Q1 Kindly advise following information of INA180A3QDBVRQ1 , thanks.
Location of wafer manuafacture:
Process of wafer (unit: nanometer/micron):
Size of wafer:
Back end manufacture:
Location of back end:
Package supplier name & location…
Part Number: INA180-Q1 Other Parts Discussed in Thread: INA190-Q1 , INA186-Q1 Hi team,
Is it possible to set low pass filter on amplifier OUT like below?
The maximum capacitive load on a D/S is typically 1nF, so I was wondering if the 10uF of the low pass…
Part Number: INA180-Q1 Other Parts Discussed in Thread: INA180 Dear tech support,
we use the INA180A4QDBVRQ1 component in one of our product - the product is validated and it is currently in production (hundreds of units in the last 3 years - Motorsport…
Part Number: INA180-Q1 Other Parts Discussed in Thread: INA180 Hi Team,
Could you please check the ICC based on Temp(3- points)?
LG IT is going to developing new Lidar project and need this data to discuss it with OEM.
-40 degree
25 degree
85 de…
Part Number: INA180-Q1 Other Parts Discussed in Thread: INA180 Hello Team,
Could you please check if GAIN4 is correct when applying current sensing and resistance
(now they are setting with Gain 4)
INA180A1QDBVRQ1 (IC6 apply): R84, R85 100K resistan…
Part Number: TLV6001-Q1 Other Parts Discussed in Thread: TLV9001-Q1 , INA180-Q1 Hi,
Customer would like to use TLV6001-Q1 as Diff. Amp as below circuit.
Is each R value correct when using Diff. Amp?
If the value is wrong, please check the recommended value…