Part Number: INA219 Hey Team, Astera Labs is currently working on a project and is using the INA219. Could you please review?
Here is the schematic: TI_review.pdf Thanks, Joey
Part Number: INA219 Other Parts Discussed in Thread: TLV709 We have a product with the INA219 being solely used for bus voltage monitoring. The IN+ and IN- terminals are shorted together on the board since we don't want to use a shunt resistor or current…
Part Number: INA219 Tool/software: Hi,
I have 4 INA219 connected to single I2C SDA and SCL line - like in a fanout way. What pull up resistors on SDA & SCL line I should use to get the values for all 4 INAs?
Thanks,
Tanveer
Part Number: INA219 Other Parts Discussed in Thread: INA220 Hi Experts,
We are using INA219 to perform Voltage and Current Measurment
The voltage reading is OK (~12V) – Reg 02
The current (shunt voltage – Reg 01) reading gives results which is higher…
Part Number: INA219 Tool/software: Hi,
I am using INA219 to get bus reading and I am not sure if this device is causing any issue to my 3.3V LDO.
I have it on the input side of LNA. The supply voltage to INA219 is 3.3V but the shunt resistor going…
Part Number: INA219 Tool/software: Hello,
Is there a maximum current rating for the INA219 chip?
I'd like to use it in my design, and I'm pretty sure it'll be more than fine for the 130mA I'd like to monitor, but I just want to make sure.
Thank…
Part Number: INA219 Other Parts Discussed in Thread: INA226 , SYSCONFIG Tool/software: Hello we are using the TI INA219 with a STM H7 Nucleo reference board over I2C. Questions:
1. Are there any sample device drivers from TI for using TI's INA219 over…
Part Number: INA219 Other Parts Discussed in Thread: TMS320F280039C Hello,
I am using an INA219 DC current sensor module to measure bus voltage, shunt voltage, current, and power through I²C interfacing the INA219 with a TMS320F280039C LaunchPad using…
Part Number: INA219 Tool/software: Hi,
We have implemented multiple INA219 shunts to monitor up to 10A current on multiple circuits.
The circuit uses a fuse with known resistance (5 mOhms) as the shunt resistor, everything else is standard reference…
Part Number: INA219 Other Parts Discussed in Thread: INA226 , SYSCONFIG Hi,
Does there have sample code for INA219? Would you please share to me? thanks!
Jeff