Part Number: INA302-Q1 Other Parts Discussed in Thread: TINA-TI
Hi team,
I simulated the start up behavior using TINA-TI model on TI.com and found that there is about 150us start up delay
only when I connect REF to GND(this is my use case).
If I apply…
Part Number: INA302 Team,
A customer would like to monitor current and would like to have different curent levels for which an alert should be generated. To achieve this, the idea would be to use two INA302 in parallel.
Is there anything that needs to…
Part Number: INA302
Dear Amplifier Team,
could you kindly help me with the foloowing information for the INA302
1. The maximum recovery time of the output stage from the saturation (both supply rails)
2. How to consider the reference voltage or its influence…
Part Number: INA302 Other Parts Discussed in Thread: TIDA-01590 , INA260 , TIDA-01065
Hi
I am designing 115VAC switch with mosfets(back-to-back configuration) and I want to measure load current with INA302A3. Can I use mosfet’s driver isolated ground in…
Hey Egoitz,
There is no way to deactivate or lessen the hysteresis.
The INA301 with a VLIMIT of 50mV is not a recommended application not only because it VLIMIT is close to they absolute hysteresis, but also because Vout at 50mV is close to the swing…
Part Number: INA302 Hi,
We have implemented INA302 for over current protection in our design.
The LIMIT2 is set for 40A current limit. The LATCH2 pin is tied to GND (Transparent mode)
The Delay pin has been connected to a 10uF capacitor to provide 2.44s…
Part Number: INA302 Other Parts Discussed in Thread: OPA333 , INA226 As per this design Guidelines
* It says input of max of 400V (Is that referring to DC /AC)?
* I did not understand use of Rz with Zener Diode since Zener Diode will have Dynamic resistance…
Part Number: INA381 Other Parts Discussed in Thread: INA303 , INA302 , INA300 1m ohm shunt is used to measure current. 2 INA381 ICs are used to measure bidirectional current in battery for charge (6A) and discharge (110A). When ever Surge is applied across…
Part Number: INA302 HI TI,
I need over current protection for AC.
Please refer to below block.
My concept is disconnect from ac line when the current flow above the threshold i set. (2A)
You can also suggest another solution without an opto-coupler…