Part Number: INA901-SP As I read the datasheet, current sensing of I*R less than 20mV cannot be expected for low voltage supplies when VCM is less than or equal to VS, the supply voltage (Section 7.4.2.4).
Is that correct?
I am trying to evaluate using…
Part Number: INA901-SP Other Parts Discussed in Thread: TPS7H4001-SP
Hello,
If I were to use a switching regulator to power a 1V@15A FPGA, then the output pins from the POL would be connected together to a power plane. This would be sized to ensure it…
Part Number: INA3221 Other Parts Discussed in Thread: INA901-SP Tool/software: Hello,
I would like to have voltage, temperature and current monitoring solution on the PCB which is under development. The voltage level is 3.3V. The temperature range is…
Part Number: INA901-SP Hi Team,
I have following request, can you please check and advise?
"
I couldn't find a report on single event effects for the INA901. There are TID and Displacement Damage reports in the system. If possible, can you send the…
Part Number: INA901-SP Hi all,
I am currently working on a project using the INA901-SP with two decoupling capacitors wired as shown below:
My question is whether I can have one of these decoupling caps on the bottom layer to optimize space as follows…
Part Number: INA901-SP Other Parts Discussed in Thread: INA240 Hello Team,
Good day.
My customer wanted to confirm if the 5962-1821001VXC rad tolerance enough to cover our requirement? Their requirement is TID below 1Krad and it is pity to use the rad-hard…
Part Number: INA240 Other Parts Discussed in Thread: INA901-SP Tool/software: Hi,
Just wondering why INA240-SEP part is pulled out from TI? Is availability foreseen in the future?
BR,
MIka Hirvonen
Part Number: INA190 Other Parts Discussed in Thread: INA901-SP
Hi team,
Ian Williams indicated in this post that the INA901-SP has moved to inactive status and will return to production later this year. Based on that I have two questions:
1. Is there…
Other Parts Discussed in Thread: INA901-SP We understand the 5962-1821001VXC has not been delivered yet. Due to the issue discussed in CE9-P-20-02, the part is being re-characterized and the SMD will eventually be updated. Did TI sell any flight parts…
Part Number: INA168-Q1 Other Parts Discussed in Thread: INA901-SP , , INA168
I am trying to compare some things between the INA168-Q1 and the INA901-SP (5962L1821001VXC). The INA168-Q1 does not exist in the "Current Sense Amplifier Comparison and Error…