Part Number: ISO1212 Other Parts Discussed in Thread: ISO1211 HI. I used the component in the STO (safe torque off) circuit.
I am in the process of product certification and need to know if the ISO1212 component has a common point of failure between…
Part Number: ISO1212 HI,
I'm using ISO1212 Digital Input IC to support current sink and source feature (24V input) without changing any assembly options. Below is portion of DIN schematic for review. Kindly review and let me know if any changes is required…
Part Number: ISO1212 Other Parts Discussed in Thread: PSPICE-FOR-TI We need the Spice model of the chip ISO1212 for the circuit Simulation. I could download the PSpice model from the TI website but converting from PSpice to the Spice is creating the following…
Part Number: ISO1212 Hey team,
Is the ISO1212 spice model encrypted? I couldn't tell as this article mentioned a file that's not in the zip file. https://e2e.ti.com/support/tools/simulation-hardware-system-design-tools-group/sim-hw-system-design/f/simulation…
Part Number: ISO1212 Hi
1. If we chose: Rsense (560ohms), Rthreshold (1K) and Rshunt(100K). Which resistor size would you recommend for Rthreshold and Rshunt? We would like to know so we can properly choose the power rating of the resistors.
2. How…
Part Number: ISO1212 Other Parts Discussed in Thread: ISO1211 Dear members,
As I'm working on VAC detection circuit, I found this chip. it can help me perfectly make the circuit. I wanted to know if there is possibility to design the exact value, I…
Part Number: ISO1212 Hello,
Here is the design requirement of threshold ON & OFF as below.
Threshold_ON setting is ok with 15V, but Threshold_OFF is NG it's about 13.8V. Could you help to clarify why with the setting below, the threshold_OFF can…
Part Number: ISO1212 if i caculate Rsense andRthr power consumption refer to I(INx+SENSEx) ,P(Rsense)=I2R=(2.47mA)2*562R <1/16W P(RTHR)= (2.47mA)2*1K<1/8W
It will be enough for Rsense using 0402 power consumption and Rthr using 0805
but if i caculate…
Part Number: ISO1212 As a one of our project Implementation, we planned to use ISO1212
To sense the dry contact Input signal which are in the range of 12V & 24V.
So, could you please suggest the reference circuit with component details including…
Part Number: ISO1212 Other Parts Discussed in Thread: ISO6721 , ISO7720 , ISO1211
Hi ISO team,
I saw the ISO1212 VIH and VIL Calculation formula is shown in blow from datasheet.
We can see in the Calculation formula, 8.25V and 7.1V is ISO1212…