Part Number: ISO7221M Other Parts Discussed in Thread: ISO7721 , ISO6721 , ISO7421 , ISO7521 , ISO7821 , ISO7421E-Q1 , ISO7021 Team,
For https://www.skyworksinc.com/en/products/isolation/si84xx-digital-isolators/si8422bb-is Our cross ref tool does list ISO7721…
Part Number: LMG3522R030-Q1 Other Parts Discussed in Thread: ISO7721 , ISO7741 HI, we are working on a inverter design with the LMG3522R030-Q1 to be used with Li-on batteries. We have made a rough board with just the H-bridge to test the GAN-FET devices…
Hello to both of you (Mr. Jonny and Mr. Jonathan),
I am working on isolated bridge DC/DC converters, in which each switch requires short circuit protection. In case we are using LMV762 with negative biasing, it may give negative output which will become…
Hi Hitoshi-san,
Yes, ISO1042-Q1 should be the optimum solution as this integrates both isolation and CAN transceiver in a single chip.
Regarding the 2-channel digital isolators, I would like to clarify that ISO72xx and ISO77xx are two completely different…
Hi Azhar,
Thanks for your interest in ISO7721-Q1.
This is a very broad question, it would be best if you can let us know if is any particular EMC test (one or more) that you like us to refer to while answering this question?
Assuming the question is associated…
Part Number: ADS7951-Q1 Other Parts Discussed in Thread: ISO7721 Hello All,
1.what is the Ti recommendation for ADS7951-Q1 ADC for the below pins?
1.Unused GPIO
2.NC pins
3.Unused ADC Channel
2. what is the Ti recommendation for unused channel in the…
Part Number: ISO7721 Other Parts Discussed in Thread: TXB0104-Q1 , Dear Team,
The customer originally using TXB0104-Q1 with TSSOP14T package.
But they are facing some issue so they move the solution to ISO7721.
The test result is good with fly wire.
Do we…
Part Number: LMV762Q-Q1 Other Parts Discussed in Thread: LMV762 , , ISO7721 , ISO7720-Q1 Hai,
I have a doubt regarding the biasing supply voltage of LMV762 comparator. Whether we can apply negative biasing voltage for this comparator? In the datasheet …
Part Number: ISO7741-Q1 Other Parts Discussed in Thread: ISO7721-Q1 , Good morning team,
I am working on an application with ISO7741-Q1 and ISO7721-Q1. In this system, during sleep mode, the supplies will be turned off and some of the input/output digital…
Part Number: ISO7721 Other Parts Discussed in Thread: TPS1H000-Q1 , TPS4H000-Q1
Hi everyone,
I have an application for my microcontroller application. I need to enable some pins related with microcontroller but I don't want to use optocoupler. Instead…