Part Number: LM101AJAN Other Parts Discussed in Thread: LM101AQML , Hi
What does the 5D on this product marking mean? We bought it in 2D before
Is there any difference between these two marking functions
Please help to confirm
T hank you.
Part Number: LM101AJAN Do any drop-ins exist for LM108s? Preferably automotive grade.
Also, side question, have super-beta transistors been phased out in creating of super gain op-amps?
Part Number: LM101AJAN Hello,
We had developed below schematic for the requirement.
U1 : Voltage follower
U2 : I to V converter
The desired output we expected is 16V to 18V based on the intensity of light falling on RX1 , but the output is showing…
Part Number: LM101AJAN They are using LM101AJ device with a single rail +15.5V supply. The absolute maximum supply rating is +/-22V.
I would have expected absolute maximum 'Input Voltage' to be to its supply rail (+15.5V in this case), however it is…
Hello Renan,
I believe that the first two products are available and orderable (I just think that the part numbers are slightly off and not actual part numbers).
Instead of M38510/10103BCX, i think it is M38510/10103BCx where the small x is a wildcard…
Other Parts Discussed in Thread: LM101AJAN , LM101A-N Hi all,
I am looking for an equivalent alternative to replace the old operational amplifier LM101AJ8 (CDIP package, 8 pins).
As option 1, I have found the LM101AJAN as best alternative. Orderable…