Hey Arjun,
The converter can be 20 Vin and the controller can take in a different voltage. LM117QML-SP is an option in space grade devices to take the 20 V input down to a different voltage.
https://www.ti.com/product/LM117QML-SP?keyMatch=LM117-SP
Thanks…
Hey Doug,
While the controller has a supply input of 14 V, since its not in the way of the high power path, you can simply bring the input down with an LDO, such as the LM117QML-SP. https://www.ti.com/product/LM117QML-SP Our plastic space options for LDOs…
Hello Guys,
Thanks for looking into this.
By the way customer is using the LM117QML-SP (SNVS356D) datasheet. But I think the answer above still holds true.
Could you help check if the following computations are correct?
1. His operating environment is…
Other Parts Discussed in Thread: MKT-WG16A-MS , MKT-WG10A-MS , SN0020HKH , SN0010HKU , SN00020FK Looking for mechanical package samples for trim and form setup
Answer:
For our Power Ceramic QMLV qualified portfolio of devices we do offer the following mechanical…
Hi Tilman,
Welcome to E2E Design Support Community!
We are actually working on updating our TI Space Products Guide (ti.com/spaceguide) to include a list of Dummy Packages / Mechanical Samples, which should be updated in the coming months. In the meantime…
Part Number: LM117HVQML-SP Other Parts Discussed in Thread: LM117QML , LM117QML-SP hello
i have a few more questions about regulator LM117H MDE.
1. what is the thermal resistance of LM117H MDE as it in DIE configuration ?
2.is the junction temperature…
Part Number: LM2941QML-SP Other Parts Discussed in Thread: LM2941 , LM117QML-SP , TPS7A4501-SP , TPS7H1101A-SP , LM117 Hi all,
On the first page of the LM2941 datasheet is highlighted that this component can adjust it's output from 5V to 20V.
Is it possible…