Part Number: LM119 Dear Sir/Madam,
I'm interested in the LM119H and would like to enquire more information
1) The process technologies, eg bipolar, cmos
2) datasheet mentioned HBM tests for ESD, was CDM perform by the company?
3) what is the MSL…
Part Number: LM119
When I try to access the 2-Factor Authentication for QCI, I get his message, after inserting my user name and password into their respective fields. I am prompted for a passcode. Can I get a passcode? Can I possibly get a phone number…
Hi Shunsuke,
The LM119 is on a classic junction isolated bipolar process and does not have thyristor or SCR structures found on CMOS products. Single-Event Latchup would be unexpected. SEL testing of the LM119 done by NASA can be found by searching on…
Other Parts Discussed in Thread: LM119 In a application, the LM119 inputs were accidentally pulled as much as 30V below -Vcc pin. What is the maximum voltage that the inputs can be below -Vcc before the input transistor fuse short? I have reviewed the datasheet…
Other Parts Discussed in Thread: LM119 Honeywell looking to drive the input of an LM119 with +/-15V signal powered off of single 5V supply. The LM119 datasheet seems to indicate that the max input voltage is VDD (5V in this case). However, there is a quest…
Part Number: LM119QML-SP Other Parts Discussed in Thread: LM139-SP Customer would like to use LM119-SP but spec indicates that the positive power supply input should not be more than 16V above ground pin voltage. In their case, they have a 23.5V power…
Other Parts Discussed in Thread: LM119 , LM339 Looking for information from users of the LM119 LM219 LM319 or experts on the internal circuitry of the LM319.
Inherited a LM319 circuit used to detect if an input is above or below +12V (other input has pullups…