The only space-rated 3-V comparators are the TLV1704-SEP and LM139-SP.
A plain TLV170x is neither constructed nor tested for radiation tolerance. Do you want to risk it anyway?
Part Number: LM139 Hello,
I can't seem to find this info on the datasheet, but what is the difference between these three part numbers?
LM139 MD8
LM139 MDE
LM139 MDR
Thank you!
Part Number: LM139-MIL Other Parts Discussed in Thread: LM139AQML , LM139 , LM139A Dear All,
I've a question about LM139-MIL available packages.
In first page of datasheet there is a table reporting the available packages of component and there is also…
Hello Yenwu,
We can only speak for the Amps and Comparators. The Power and Logic devices should be posted to the approprite forums.
For the LM211 and LM193, they are fab'ed on a high voltage junction Isolated bipolar process. Feature size is proprietary…
Part Number: LM139AQML-SP Other Parts Discussed in Thread: LM139 , LM139A Team,
I just wanted to make sure that the below ordering reference is for the die version: LM139 MDE : 5962R9673802V9A ( http://www.ti.com/product/LM139AQML-SP
Part Number: LM139 Other Parts Discussed in Thread: TLV7011 If I’m holding one input at the midpoint by two identical resistors. Like two 1k resistors so the reference level input is 3.3/2 = 1.65V and the other input will swing up and down 0v to…
Part Number: LM139 For LM139,if supply voltage is'V', what is the recommended maximum input voltage at + and -ve inputs?if supply is 6.4v and +ve input is 3v,can we apply 11v at -ve input?will it be recommended operating condition?
Part Number: LM139 hi,
What should I do with the unused input pins for the LM139?
I read through the datasheet and it doesn't mention what to do with any unused pins. A datasheet for a similar part said to tie all unused input pins to the negative…