Part Number: LM211-EP Other Parts Discussed in Thread: LM111 Is input offset voltage expected to shift as a device ages during extended storage with conditions within those specified on the datasheet?
Is output voltage expected to shift as a device ages…
Part Number: LM211-EP Is input offset voltage expected to shift with temperature? Is the direction of shift expected to trend with temperature (ex: shift up with high temperature, and shift down with low temperature or the reverse)?
Is voltage output…
Part Number: LM211-EP
Hi Team,
See the question below:
Can you confirm the lead composition and finish on LM211MDREP as noted on the TI Reliability report located at: https://www.ti.com/lit/pdf/sglk019
I believe it would be unusual to have a lead composition…
Part Number: LM211-EP Hello Team,
I understand the worst-case common-mode voltage input for proper operation is VCC– + 0.5 (min) and VCC+ – 1.5 (max). Is this requirement that both inputs need to be within this range or only one input needs to be in…
Other Parts Discussed in Thread: LM211-EP I would like to know that LM211-EP setting.
I would like to set VCC+/- are +/-5 and Vout connect resister to gnd. Because Vout swing level from gnd to over +3V.
Does it work correctly with those settings?
Part Number: LM211-EP Other Parts Discussed in Thread: TL331-EP Team, Can you help with the below questions:
Saturation Voltage of the output BJT
The datasheet specifies it at 0.23, typ to 0.4, max at 8mA. Do you have data on what we should expect when…
Part Number: LM211-EP Other Parts Discussed in Thread: LM211 Hi,
I need Junction to Case Thermal Resistance (Rjc) and Junction to board Thermal Resistance (Rjb) details for LM211MDREP component. It appears that the data sheet only has junction to ambient…
Part Number: LM211-EP Other Parts Discussed in Thread: LM211 Hi team,
Good day. Our customer is requesting for the ESD HBM rating for LM211MDREP. Is the ESD HBM rating of non-EP version which is LM211 applicable?
Regards, Carlo
Hello Zoe,
As Clemens showed, there are just the Military versions available of the LM319 that extend the temp range, and in large packages.
The die is too big to put in a TSSOP.
The similar output single channel LM211 is available in commercial, Q1 and…
Part Number: LM211-EP Other Parts Discussed in Thread: LM311-N , LM211 , LM111 I need to use the Strobe function, but not the Balance function. The note in Figure 12 says that if balancing is not used, then BALANCE and BAL/STRB pins should be shorted together…