Part Number: LM2901AV-Q1 Dear All, I need information. Can you tell me if LM2901AVQDRQ1 could have altitude related problems? Does the component continue to work well at 6500 m?
In general, what are the altitude related issues for an electronic component…
Part Number: LM2901AV-Q1 Dear All,
I've a question about maximum output current (per comparator) of LM2901AV-Q1.
In datasheet it's reported that the "Recommended max output current" is 4mA. What does this means?
Can't I use it at 6-7mA? What happens…
Part Number: LM2901AV Other Parts Discussed in Thread: TL331 , LM397 , LM2901 , LM2903 , LM393A , LM293A Dear Team,
We are using comparator of part LM2901AVQPWR in our design.
The above comparator is 4 channel, we need similar comparator with 2…
Other Parts Discussed in Thread: LM2901AV , LM2901 , TLV3011 Dear sir or madam
We are using the LM2901AV and the datasheets requires that the Common-mode input-voltage range stays below Vcc-2V.
My questions is: How do I calculate the Common-mode…
Part Number: LM2901AV Dear All,
I've a question about LM2901AV comparator, because I've some difficult to undestand p/n construction.
In particular, what is the differences between these p/n: LM2901AVQDR and LM2901AVQDRG4?
In general, what is the…
Part Number: THS6232RHFEVM Other Parts Discussed in Thread: THS6232 ,
Tool/software:
Hi, I'm currently looking to implement an ARINC 429 transmitter.
A basic functional overview would be, a controller sends a signal that swings 3.3V to GND and the…
Part Number: LM339 Other Parts Discussed in Thread: LM2901V , LM239A , , LM139 , LM139A , LM2901AV , LM239 , LM2901 , The LM339 data sheet (SLCS006T) states (Section 8.3 Feature Description): "The output NPN sinks current when the positive input voltage…
lm139.pdf
hi,
Attached is the datasheet I’m using, I couldn’t find any information in it regarding what to do with unused input pins. I’m hooking the positive supply to 15V and the negative supply to ground.
Regards,
Eric
Part Number: LM2901 Other Parts Discussed in Thread: TLV1704 , TLV1701 , LM339 , LM393
Dear Sir, please answer
There is feature description from LM2901 datasheet, page 10: "The output NPN sinks current when the positive input voltage is higher than…