Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903B-Q1 , Hi team,
I searched datasheet that those PNs different is Device Marking. will it affect the function or application?
BR,
Jimmy
Part Number: LM2903-Q1 Hi, Team
Hope you are doing well!
For LM2903-Q1 family, I have two questions:
Q1: Which category does LM2903VQPWRG4Q1 belong to in the following table?
Q2: What are the part number corresponding to "A" Devices and "AV" Devices?…
Part Number: LM2903-Q1 Hi team,
Could you pls help clarify, if customer V+ is 12V (within 36V rating), IN- is below (V+ )-1.5V, can IN+ go up to beyond (V+ )-1.5v, eg 18V? Device still functions normally in this case, right?
Thanks
Scarlett
Part Number: LM2903-Q1 Hello Team,
What is the sinking current of LM2903-Q1 IC??
Shall i consider sink current is same as output current??
Regards,
Giridhar.
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM2903 Team,
I'm assuming that the LM2903's output is high impedance when unpowered, but don't have one here in the lab to double check. Can you please confirm?
Thanks!
Greg
Part Number: LM2903-Q1 Other Parts Discussed in Thread: LM339 Dear expert,
There are some questions about how to handle IN+/IN- when VCC is unpowered.
Output state when VCC is unpowered?
Can IN+ or IN- connect with 5V directly without any input resistors…
Part Number: LM2903B-Q1 Other Parts Discussed in Thread: TINA-TI Hello i'm using a LM2903BQ1 as a comparator. On the inverting input i have a constant voltage of 9,5V and i am compared a PWM Signal (1.7kHz by 50% Duty Cycle) with a max. ampitude of 14V…