Part Number: LM2904BA-Q1 Other Parts Discussed in Thread: TLV9002 , LM2904BA Tool/software: Dear Team,
We are using above mentioned OP-Amp ( LM2904BAQPWR1 ) in our proto circuit.
The supply voltage for the IC is 3.3V.
When we are testing the Op-amp, It is…
Part Number: LM2904BA Other Parts Discussed in Thread: LM2904 , LM358 Hi,
The LM2904 and LM358 are released in B and BA versions, respectively. As far as I can see from the datasheet, the only difference between these is the offset voltage. Are the B and…
Hi Jerry,
Thanks for confirmation. Previously, we used LM2904BA-Q1, but met the issue.
As below circuit, our VDD is 3.3V and V+ is 5V. I expected that the pin1 is 3.3V because the Vout would be clamped at 3.3V. But Vout here was only 2V.
Do you have…
Part Number: LM2904B-Q1 Other Parts Discussed in Thread: LM2904 , LM2904B , LM2904BA Dear team,
What does ”device marketing“ mean? What is the difference between these device besides different package type? I can't search for example 2904AVQ or…
Part Number: LM358A Other Parts Discussed in Thread: LM358 , LM358B , LM2904B , LM2904BA , LM358BA , Hello,
The data sheet of LM358 family (SLOS068AA) has a functional block diagram in the section 8.2 Functional Block Diagram , but is it applicable to the L…
Hi Fermo,
To add to Clemens' comments, the better low-cost solution would be the newer version - LM2904B / LM2904BA, which has improved offset and offset drift drift specs to the LM2904.
If offset/offset drift is a critical parameter, you can also…
In the LM2904-Q1 we have different voltage swing output
-for LM2904-Q1, LM2904AV-Q1, LM2904V-Q1 we have
and for LM2904B-Q1 and LM2904BA-Q1 we have
This means the output voltage swing are quite different.
Part Number: LM2904-Q1 Other Parts Discussed in Thread: LM2904BA-Q1 , Hi,
Customer have a question about datasheet for LM2904-Q1 and LM2904BA-Q1.
As showed in the following figure, why the test condition of output swing from rail differs from each other…