Part Number: LM2907-N Hi,
my customer wants to use LM2907MX-8/NOPB in an SMT production line. The datasheet specifies an infrared soldering temperature 220 degC.
however for an lead free SMT soldering process the following parameters are required:
238degC…
Part Number: LM2907-N Hello,
I'm using LM2907 IC for frequency to voltage conversion. Now I need to calculate the power dissipation of the IC.
I have calculated the power consumption P= Vcc* Icc. According to the absolute ratings, maximum power dissipation…
Part Number: LM2907-N Hello,
On page 4 of AN-162 I believe there is supposed to be an equation for selection of R1.
It seems to be missing, is anyone able to provide the equation or update the file?
Part Number: LM2907-N
1. What is the minimum supply voltage for the 2907 8-pin? I saw a post on this forum saying 6 volts, but I cannot find that in the data sheet (page 5 says -28 to 28V.
2. What is the minimum and maximum input voltage of the frequency…
Hi Jim,
I expect with the correct filter at the LM2907-N output you would be able to improve the output voltage ripple and response characteristics. TI produces the LM331, which is described as a Precision Voltage-to-Frequency Converter, but it may also…
Part Number: LM2907-N In the LM2907-N datasheet, their are parts (C1, C2, R1, Rload) and currents (I2) that are referenced; however, those parts are not referenced on any figures shown later in the data sheet. Could someone correlate which parts and currents…