Part Number: LMP8646EB Other Parts Discussed in Thread: LM3102 , LMP8646 Hi, I'm working with LMP8646EB evaluation board suggest from TI engineer Amy Le with his very interest video, anyway connect and test the board something seem not to work properly…
Part Number: TPS54231 Other Parts Discussed in Thread: TPS7A8300 , , TPS54531 , LM3102 , TPS562200 Hi ,
Please advise how to maximise the transient response of the TPS54231TPS54531 current mode control IC as it dip and ring with large spike due to sudden…
Other Parts Discussed in Thread: LM3102 , TPS54140 , LM5001 Hello
I have 18V(0.8Amp)/-18V(0.6Amp) rail with common ground (please see attached picture) and I need to buck+18 to +8 and -18V to -8V. Since I have a common ground that means I need a negative…
Other Parts Discussed in Thread: LM3103 , LM3102 , LM3100 , LP38798 , TINA-TI , I require afore mentioned files for my work, can anyone please suggest me from can I get that.
Hello,
I would like to do something similar to what you describe. In my case I have two inputs (+15V and -15V), and a common ground. I was going to use a LM3102 (or something similar) to produce +5V from the +15V input line. In theory, I can use a slightly…
The LM3102 is a 2.5 amp device. The LMR24220 is a two amp device and comes in a BGA package which can reduce the size of the design.
Take a look at the following reference design for a compact layout.
http://www.ti.com/tool/lmr24220rb
Regards,
Marc
Other Parts Discussed in Thread: LM3102 , LM20133 , LMP8646 , LMP8646EB 1. Two feedback connections are shown in the document -- one in the application information (feedback is connected to Vin- on op-amp) and one in the EVB schematic itself (feedback is…
Other Parts Discussed in Thread: TL2575-05 , LM3102 , LM2675 I need positive and negative 5v from a symmetric 30vDC supply on an amplifier project, its got to be simple and efficient with easy to solder packages, the TL2575-05 looks suitable but its not…
Hello Guilherme,
When using WEBENCH design, you got to use the exact BOM or close. If you deviate from the WEBENCH generated the BOM, there is no guarantee the device will function normally.
It's difficult to tell why the device burned up without seeing…