Part Number: TPS23523
Tool/software:
Hi Guy
We have used TPS23523 solution to design hotswap & ORing.
Our electrical parameters are as follows~~
Pin : 780W
Vin : 54V+/-10% ( 48.6V ~ 54V ~59.4V)
Iin : 16A
Cin : about 470uF
Question…
Hi Alex,
I actually made a mistake in my previous email - I'm not familiar with all of these acronyms and combined two of them! My previous answer was for SET (Single Event Transient) testing. The product engineer doing the radiation testing sent me…
OK,I understood the drive capability of TXS0108.
But we found the other question:
The I2C interface after TXS0108 level shifter can communicate with M24512 , but can not communicate with PCA9655E .
What is the reason ?
PCA9655E-D.PDF M24512-RMN6TP…
tlc3702 (working).pdf
The photo is the reel we ordered and has the non-linearity issue. Is the attached datasheet (pdf file) the correct datasheet for the reel? If not, please send me the datasheet representing the part on reel. Thank you. Jay
Dear Eric
Thanks for your feedback and suggestion, please check reply as follows and update schematic for attached file.
I see WAKE is tied VBAT through a resistor. This is okay, but the local wake function won't be available, and I want to verify…
Dear Patrick,
Here is excel design file you asked. Please check it.
LDC_Tools01.xlsx
And customer said that they will use LDC3114-Q1 as Raw Data Mode, so they will not use INTB function.
Best regards,
Chase
Tom,
Attached are two XOs families i am considering to use.
I prefer using the LVDS in order to save the terminations.
According DS Tr is up to 350pS (20/80%) while CDCM6208 guarantees 300pS (at +/-100mV) while LVDS. is that acceptable?
PNs i…